hello
Our Customer is working with the DS100MB200 and there seems to be difficulties in understanding the truth table (Table3).
In the pin description on page 4 it says that when SEL0, SEL1 are at a '0' it selects B Channel input and output. '1' in these…
Hi,
I would not recommend the DS100MB201 for 10 Gbps operation - the MB203 products work better.
All of these parts can use either pin mode or an SMBus mode of operation.
The DS100MB201 does only support 2.5V VDD.
Regards,
Lee
Hi,
The SN65LVCP114 is twice the density of the DS100MB203, so only one device would be needed. Two DS100MB203 devices would be required to create a quad 1:2 2:1 function.
I would not recommend the DS100MB201 it is an older device.
The only other option…
If you are looking to buffer a clock after it has gone through 300mm of cable, the DS15BR400 would be a good product - but it is a buffer with one input and one output per channel. If you are looking to generate additional copies of the clock, then some…
Other Parts Discussed in Thread: DS92LV2412 , DS32ELX0421 , DS32ELX0124 , DS30EA101 , DS100MB201 Hi, Is there any deserializers that can be used in a multidrop configuration ? Configuration: Data source (FPGA) ~800Mbit-1300Mbit/s The same signal will be broadcasted…
Other Parts Discussed in Thread: DS100MB201 Hi,
Our Customer is working with the DS100MB200 and there seems to be difficulties in understanding the truth table (Table3).
In the pin description on page 4 it says that when SEL0, SEL1 are at a '0' it selects…