Part Number: DS110DF1610 Other Parts Discussed in Thread: DS250DF230 Hello, Can DS110DF610 output the recovered clock from the CDR block to CLK_MON_P/N pins? If not, any other re-timer devices that can do that? Best regards, K.Hirano
Part Number: DS125DF1610 Other Parts Discussed in Thread: DS110DF1610 Tool/software: DS125DF1610 and DS110DF1610 are 16-channel retimers which implement 4x4 crosspoint switches.
There are 2 registers which need to be configured to use the crosspoint…
Hi,
For default setting, if the retimer channel CDR is not locked its output will be muted (i.e. turned off)
Regards,
Rodrigo Natal
HSSC Applications Engineer
Part Number: DS110DF1610 Tool/software: WEBENCH® Design Tools We use ds110df1610 to make a layer of wire card.The test connection is as the pic.
When the port is connected, it is found that the first port and the second port of the switch cannot link…
Part Number: DS110DF1610 Other Parts Discussed in Thread: DS125DF1610 , SIGCONARCHITECT Hi Team,
According to the datasheet of ds110df1610, the customer is not sure which registers should be set for its divider settings. Is the 0x2f register a standard…
Part Number: DS110DF1610 Other Parts Discussed in Thread: DS125DF1610 , SIGCONARCHITECT For example, there is certain data rate within DS125DF1610 VCO range but it is not a standard rate. How do you setup the device to lock to this data rate?
Part Number: DS110DF1610 Other Parts Discussed in Thread: TEST2 Hi,
Customer want to check the CDR lock fucnction. The SFP output frequency is 10.3125 Ghz.
In the first test ,they set the data rate same as SFP using STANDARD data rate method. Refer…
Part Number: DS110DF1610 Hi,
Customer facing DS110DF1610 could not lock ISSUE. We are test three signal frequency as below,only the 9.95328Ghz can be locked,the other two can not and both reg 0x27 and 0x28 were 0.
10.709225 // not lock
9.95328 /…
Part Number: DS110DF1610 Other Parts Discussed in Thread: DS125DF1610 HI ,
Customer have there question as below.
1.Dose there have layout guide for ds110df1610?
2. Whether there have problem if differential output pcb trace longer than 5 inch…