Hi ttd,
Yes, you can use terminal mode for a PCIe Gen3 application. I do recommend including a pull-up resistor footprint on the ENSMB pin and headers to access SDA and SCL pins, so SMBus slave mode can still optionally be used. Having access to registers…
Part Number: DS125BR401A Tool/software: Hello:
The 9300 platform supports PCle4x1lane and PCle3x2Lane, with a total of 2 PCIE ports. The customer wants to use these 2 PCIE ports to connect to the 10G card port chip. Since RTL8126 only supports PCIE3…
Part Number: DS125BR401A Hi Sir,
Don't you have a Frequency vs. Boost amplitude graph of DS125BR401A?
Just like the Figure 1 in DS160PR410 datasheet | TI.com .
Thanks.
Part Number: DS125BR401A Hi Team,
Customer would like to design DS125BR401A.
Would you please help review question and provide your comments?
If ENSMB set to SMBUS Slave mode, will MODE_B setting still work?
Thanks for help!
Scott
Part Number: DS125BR401A Hi,
I want to use PN DS125BR401A in my new design and I have few questions:
1) can I work only with PORT B?
2)if only port B is working, the PORT A pins (in,out, EQA,DEMA) can left floating? if not how should i need to connect…
Part Number: DS125BR401A Production test without high speed signaling.
Is it possible to test the PCB where the 125br401A is used without using high speed signals??
For production test of the PCB where the 401A is placed, we don't have access to high…
Part Number: DS125BR401A Dear team,
Could you help answer below questions?
1. Will you suggest the PCIE Redriver is close to CPU or TBT?
2. Whether the 2.5GHz is corresponding to 5GT/s speed?
Thank you.
Part Number: DS125BR401A Other Parts Discussed in Thread: DS125MB203 , DS125BR401 , DS125BR800 Hi team,
4 Port SATA3.0
Originally used DS125MB203SQ, now does not need the function of Switch
The SATA signal from the source to the Redriver to the Connector…
Part Number: DS125BR401A Dear Sirs,
I have a question about the channel loss!
As below chart, if the DS125BR401A have -24dB ability and the SAS-3 controller has -24dB ability, too.
May I think the total channel loss is -48dB for BR401A and controller 1…