Part Number: DS125BR401A Dear Sirs,
I have a question about the channel loss!
As below chart, if the DS125BR401A have -24dB ability and the SAS-3 controller has -24dB ability, too.
May I think the total channel loss is -48dB for BR401A and controller…
Part Number: DS125BR401A HI Team,
customer ask that DS125BR401A can use on USB3.0 and SGMII?
or do you suggest device to apply on both Usb3.0 and SGMII.
thanks
Best Regards,
Jay
Part Number: DS125BR401A Other Parts Discussed in Thread: DS125MB203 , DS125BR401 , DS125BR800 Hi team,
4 Port SATA3.0
Originally used DS125MB203SQ, now does not need the function of Switch
The SATA signal from the source to the Redriver to the…
Part Number: DS125BR401A Hi SIr,
Could you please help to clarify when DS125BR401A running at SATA3 6Gbps, what will we read MODE_DET Status?
I read the value as 00, is it correct?
Part Number: DS125BR401A Hello,
Could you help me confirm on the below questions, thanks in advance.
1. We recommend connect the bigger loss at the channel B side as the B side have the 24dB CTLE, am I right?
2. I have checked the positive and negative…
Part Number: DS125BR401A Dear Sirs,
Here is the customer design concept.
Their application is SAS and use MiniSAS HD cable (twist +shielded) with 1m, 3m, and 6m.
In the same cascade channel, they want to use 2 pcs on each board in TX and RX side…
Part Number: DS125BR401A Hello,
Could you help me confirm on the below questions, thanks in advance.
1. We recommend connect the bigger loss at the channel B side as the B side have the 24dB CTLE, am I right?
2. I have checked the positive and negative…
Part Number: DS125BR401A Hi team,
My customer use the DS125BR401a to drive the SATA 6G signal.
In the system, the SATA signal will go through the RAID card----1.5m cable--3inch PCB trace---DS125BR401a----10inch PCB trace---HDD
They use the channel…
Part Number: DS125BR401A Hello
Has any problem for schematics? If customer would like to used Daisy-chain way to load code from external EEPROM, please help to check schematic. especially . And how to set pin26 SD_TH on normal status ? Thank you.
Part Number: DS125BR401A Hello,
I need some additional information for DS125BR401A NJY(QFN) package.
The below is from other TI device and I need the information that is marked by yellow line for DS125BT401A. Could you tell me them?
The…