Part Number: DS125BR800 Customer is testing DS125BR800 repeater for JESD204B in SMBus (slave mode).
How to tie the unused pins, such as MODE, READ_EN and ALL_DONE?
If customer is using 4 or 6 channels only, how should they be connected if permanently…
Part Number: DS125BR800 Hello,
One customer need to confirm if DS125BR800 work with PRBS31 for ibert of xilinx?Is it suitable for Aurora 64/66 encoding? According to the datasheet it should only support 10G-KR is 64/66, which is the same as Aurora 64…
Part Number: DS125BR800 Hi,
I'm having trouble using the IBIS-AMI model in an ADS simulation.
I get the following error when starting a simulation using the IBIS model including the example project:
Error detected by hpeesofsim in DS125BRxxx_Rx_AMI…
Part Number: DS125BR800 Other Parts Discussed in Thread: DS125BR820 Hello team,
Could you please check the application use case attached on the internal link here is OK?
The application is eye opener for CMOS sensor I/F.
Regards,
Itoh
Part Number: DS125BR800 Other Parts Discussed in Thread: DS110DF111 , DS125DF410 , DS125BR820 Team,
A few questions on the DS125BR800:
Can it capture eye diagrams?
How do we display the eye diagram - with a standard TI i2c dongle and some GUI application…
Part Number: DS125BR800 Usage environment: 8b10b 6.6Gbps Xilinx Aurora,
・Please tell me the settings of MODE and Rx detect of DS128BR800 that are optimal at 8b10b 6.6Gbps. Rx detection function is not used. ・Are there any precautions for the EQ, DEM, and…
Part Number: DS125BR800 Hi all
I would like to use DS125BR800 to extend SVLS-EC (Sub-LVDS) data transmition length.
Application is as follow
SONY Image-sensor ---SLVS-EC--> DS125BR800 ---SLVS-EC--> HOST.
Is it capable to use this component for…
Part Number: DS125BR800 Hello,
I am simulating the DS125BR800 redriver IBIS-AMI Model in a 8 Gbps setup using HSpice.
While I got the AMI models running, simply assining them to port-elements in HSpice, I have problems using the IBIS-part of the model for…
Part Number: DS125BR800 Hi Team,
There are two questions about DS125BR800, could you please help explain? Thanks!
1. The datasheet says "Transmit Output Voltage Control: 700 mV to 1300 mV", is the voltage peak to peak voltage or average voltage?…
Part Number: DS125BR800 Other Parts Discussed in Thread: DS125BR820 , DS125BR401A HI team,
Do we have some recommend redriver devices for SAS3.0? Thanks.