Part Number: DS125DF111 Other Parts Discussed in Thread: DS110DF111 Hi Support Team,
I am designing a product that requires a 10G network interface. My design includes a SoC with a 10G XFI interface, which I would like to connect to an SFP+ module.…
Part Number: DS125DF111 Good morning. I wanted to know if there are any specific rules regarding the section that generates the chip's power supply when using the DS125DF111 chip. I built a custom board that uses two optical SFP+s, and the DS125DF111…
Part Number: DS125DF111
Good morning TI experts.
I would like some help regarding the optimal configuration for the DS125DF111 chip, so that it can function as a RETIMER on a Xilinx Aurora 64b/66b link at 10.3125 Gbps. At the moment, it seems to work…
Part Number: DS125DF111 Other Parts Discussed in Thread: USB2ANY , Hello,
we are using the DS125DF111 on a custom SFP board in conjunction with a FPGA as the source and sink of datastream. We interfaced the DS125DF111 with the USB2ANY and SigCon Architect…
Part Number: DS125DF111 Other Parts Discussed in Thread: DS110DF410 , DS125DF410 , , DS125DF1610 Tool/software: Hi TI
we have new requirement need to evaluate for PRBS generator,
Data-Rate(Tx): ~3Gbps.
Rise/Fall: 30ps(Min) and 42ps(Max)
P-P…
Part Number: DS125DF111 Other Parts Discussed in Thread: DS110DF111
Hello,
I am planning to use the DS125DF111 in my upcoming design, and before moving forward I’d like to speak with an applications engineer. I want to confirm that this is the correct…
Part Number: DS125DF111
Tool/software:
Hello:
Regarding the application of DS125DF111. The customer has now made a test board and tried their best to debug it. The result is that the sensitivity of 10GE has improved slightly, but the sensitivity…
Part Number: DS125DF111 Tool/software: Hi TI expert,
Is there an IBIS model available for the DS125DF111? I would like simulation with ibis model
thanks
Smith
Part Number: DS125DF111 Other Parts Discussed in Thread: DS125MB203 Tool/software: Hello:
Regarding DS125MB203, the customer's application scenarios are as follows:
Function consultation:
(1) The signal source speed is 1Gbps or 2.5Gbps and 9.97Gbps…
Part Number: DS125DF111
If I change the value of register 0x07 : 0x03'h in the control/shared register set, I think it will work as loopback. Is that right?
0xff 0x00 Select control/shared Register
0x07 0x03 input A --> Output B and input B…