Part Number: DS125DF111 Other Parts Discussed in Thread: DS110DF111 , TI Design Support Team:
Please advise on DS125DF111 and DS110DF111 programming data rates (0x60-0x64).
We have designed and test the DS110DF111 at various data rates for our product,…
Part Number: DS125DF111
For some reason, when laying out the PCB,i need to set the input and output of DS125DF111 as shown in the figure, the input is OUT_P --- INA- \ OUT_N ----- INA+, and the output is also OUTA- ---- TD+ \OUTA+ ----- TD-, my question…
Part Number: DS125DF111 Hi TI technical support team,I have encountered the following problems and hope to get your help,TKS!
I have a SFP+ module project which use DS125DF111 .I use the B channel, and I am going to work at 1.25Gbps and 10.3125Gbps,but…
Part Number: DS125DF111 Hello,
i'm searching for the SigCon Architect updater file for DS125DF111,
it is not in the SNLC056A SigCon Architect Repeater Profiles v1.1 file i've downloaded earlier today.
can anyone profide me this file?
Part Number: DS125DF111 Other Parts Discussed in Thread: DS280DF810 , USB2ANY , DS280BR810 Hi team,
My questions are as follows:
1. is there a reference design under the control of MCU?
2. Under the control of MCU, is it master mode or slave mode?
3. In…
Part Number: DS125DF111 Other Parts Discussed in Thread: DS125BR401A Dear Team,
Attached for DS125DF111 transmitter eye_diagrame and Tjitter measurement using the best of de-emphasis 0x14 (-6dB) VOD setting 0x85 . I first adjusted the VOD setting within…
Part Number: DS125DF111 Hello,
I encountered an high-speed interface disconnection issue while designing DS125DF111 in SFP+ adapter card.
We founded that there is a DS125DF111EVM product for verifying usage from TI website.
However, that one uses SMA connector…
Part Number: DS125DF111 Hi TI Team,
Our client requirement is SFP/SFP+ interface (1Gbps/10Gbps). As per the design, the system implementation will be LS1046A--> Retimer(DS125DF111)-->SFP port / SFP+ port.
In datasheet fig 9 typical application is…
Part Number: DS125DF111 I use DS125DF111 as a retimer, which works at 1.25Gbps and 2.5Gbps. I need to set the CTLE in the front stage to the maximum setting. How do I set it specifically?
I setting below,is it correct?
addr data mask
0x31 0x00 0x6…
Part Number: DS125DF111 Hello, based on the DS1125DF111 transceiver data transmission module, in the case of a direct connection with a cable, the receiving end can detect and lock the signal, but with wireless transmission, the receiving end can only…