Part Number: DS15BA101 Other Parts Discussed in Thread: DS30BA101 Hi TIer
My customer want to use DS15BA101 in 2.2 Gbps, But in the chip introduction, there only show the 1.5Gbps, and in datasheet there have 2Gbps test result.
So could you help…
Part Number: DS15BA101 Other Parts Discussed in Thread: DS15EA101 Hi,
I would like to connect two devices by SGMII, 1.25G with different voltage level as following:
TX side: device 1 transmit range is 225 - 525mvp-p to device 2 receive range 500…
Part Number: DS15BA101 Other Parts Discussed in Thread: DS15EA101 Tool/software: We want to extend LVDC transmission distance to 50m, DS15BA101 can realize?
Could you give any recommend project designs. thanks!
Part Number: DS15BA101 Other Parts Discussed in Thread: DS15EA101 , Hello team, My customer has a question about DS15BA101 and DS15EA101. They are considering to use them after converting differential signal from SPI signal to expand with long cable.…
Part Number: DS15BA101 Other Parts Discussed in Thread: DP83869HM , , SN65LVDS100 Hello There,
we use DP83869HM as PHY for 100M media converter. In order to connect Optical receiver we need to meet PHY input specification of 0.3-2.0 V for differential…
Part Number: DS15BA101 Other Parts Discussed in Thread: DS30BA101 Hi,
I'm looking for options to drive clocks over long distances through twisted pair - probably CAT5. I see the DS15BA101 could be an option, however this part seems quite old and the…
Part Number: DS15BA101 Hello, My customer has questions about DC Electrical Characteristics on the datasheet as follows. Q1: Vos(typ) is specified as Vcc-Vout/2. Under what kind of test circuits this Vos should be measured? Q2: Vout is specified under…
Hi Steven,
On DS15BA101 OUT- at the moment we only have a 49.9 ohm to VCC. Can you please add another 49.9 ohm to this pin. The other side of this resistor goes to a 1uF capacitor to ground. I am checking if having a balanced impedance on OUT+ and OUT…
Part Number: DS15BA101 Other Parts Discussed in Thread: DS15EA101 , Hello,
My customer would like to connect DS15BA101 and DS15EA101 with DC-coupling and single-ended topology like the following circuit. Is this circuit correct? If not, could you suggest…
Part Number: DS15BA101 Hi
The datasheet mentions that the RVO network should be removed to minimize parasitic capacitance. If the resistance between RVO pin and VCC is controlled by digital potentiometer with 40 to 90pF as capacitance between pins of…