Part Number: DS15BA101 Hi,
we use DS15BA101SDE to be our buffer. input is LVDS and output is also LVDS, than use this IC Rvo to adjust Vod that range is 100mV to 900mV.
I had a problem because I LVDS a port is 5 pairs differential signals. DS15BA101SDE…
Part Number: DS15BA101 Other Parts Discussed in Thread: SN65CML100 , Hi, we require a CML driver for Hotlink data at 250Mbps to 800Mbps link rate and are trying to decide between the DS15BA101SD or the SN65CML100.
I like the DS15BA101SD better as it is a smaller…
Part Number: DS15BA101 Hello,
my customer is currently working on a project with the DS15BA101SD which they use as driver for a 10m long point to point connection. the output voltage amplitude was set to 800mV as specified in the datasheet. However the…
Part Number: DS15BA101 Other Parts Discussed in Thread: LMH0202 , LMH0302 Hello guys,
One of my customers is using a lot of DS15BA101 in their products. But they are in trouble on field with the device. Accoording to their information, it seems that the…
Part Number: DS15BA101 Other Parts Discussed in Thread: DS15EA101 , Hi team,
The customer would like to use DS15BA101 and DS15EA101 for the AC Coupled application.
The attach is his design block diagram.
Q1. Can DS15BA101 and DS15EA101 be used for the AC Co…
Part Number: DS15BA101 Other Parts Discussed in Thread: DS15EA101 Dear,
I would like to have a confirmation that I can use the DS15BA101 buffer to drive 25MHz and 80MHz LVDS clocks to a 50 Ohm coaxial cable that could be 2m to 10m long.
Could you also…
Part Number: DS15BA101DS15BA101SDE/NOPB
Theta JB is not provided in the datasheet, can you provide that package thermal resistance for this component?
What is the recommended operating Tj (Junction Temperature)?
Part is rated for -40 °C to +85…
Part Number: DS15BA101 Other Parts Discussed in Thread: DS15EA101 ,
DS15BA101SDE/NOPB
Theta JB is not provided in the datasheet, can you provide that package thermal resistance for this component?
What is the recommended operating Tj (Junction Temperature…
Part Number: DS15BA101 Hello,
I would like to know the behaviour of the output of the DS15BA101 if the differential input voltage is 0mV.
The input of the buffer in my application is ac-coupled and afterwards terminated with 100Ohm connected between the…