Part Number: DS15EA101 Other Parts Discussed in Thread: DS15BA101 , DS30EA101 , DS30BA101 Tool/software: WEBENCH® Design Tools Hi Team,
I would like to simulate TX/RX performance of DS15BA101 and DS15EA101 as a pair.
TX------channel----->RX
However,…
Part Number: DS15BA101 Other Parts Discussed in Thread: DS15EA101 , Hello,
I want to know coplanarity and standoff parameter of the below devices:
DS15EA101
DS15BA101
But I can’t find these information in the datasheets.
I think QFN/SON package…
Part Number: DS90UA101-Q1 Other Parts Discussed in Thread: DS15BA101 , , DS15EA101 , DS90UA102-Q1 I am working on something called a floor box in the AV community. This takes a bunch of audio inputs and puts them on a single cable then sends them to another…
Other Parts Discussed in Thread: DS15BA101 Dear Sir,
Regarding DS15BA101, our customer would like to know whether voltage biasing is required to the CML input or not. They use AC-coupling caps on the input. According to the datasheet(SNLS234J), the input …
Part Number: DS15BA101 Other Parts Discussed in Thread: DS90UB933-Q1 Hi all,
As the title suggests, I would like to know whether it is possible to extend the STP cable length of the DS90UB93{3,4}-Q1 SerDes pair to 50+ meters by placing the DS15{B,E}A101…
Hi Mark,
I reviewed the datasheet and compared it with the DS30BA101. You are correct, the device is designed to drive a 50-ohm load for each polarity, so the spec should be for 50 ohm load instead of 25 ohm load.
Thanks,
Michael
Other Parts Discussed in Thread: DS15BA101 Dear Support team,
I have some question regarding DS15BA101.
When "IN+" and "IN-" are opened, we found the phenomenon what the OUT+ and OUT- have the vibration by itself.
“IN+” and “IN-“ are…
Other Parts Discussed in Thread: DS15BA101 , DS15EA101 Dear Sirs
I use TI DS15BA101 for cable extended application. (30m)
But the LVDS signal will be reduced to below 250mV on recevier DS15EA101 and the signal quality is bad.
I have set DS15BA101 Rvo to 487Ω…
Other Parts Discussed in Thread: DS15BA101 , DS38EP100 , HD3SS3411 , DS15EA101 Hi, TI supporting staff.
Currently I try to apply DS15BA101 as Receiving side signal buffer for high speed transmission.
But the DS15BA101 doesn't have enable of shutdown pin…
Other Parts Discussed in Thread: DS15EA101 , DS15BA101 , DS30BA101 Dear Sirs
I use DS15BA101 or DS15EA101 for cable extended application.
The LVDS max output signal is 400mv.
Does TI provide similar IC but LVDS max output signal is 500~600mv?
Thanks
BRS …