Other Parts Discussed in Thread: DS92LV16 , DS15BA101 , DS15EA101 , DS92LX1622 , DS92LX1621 , DS92LX2121 , DS92LX2122 , DS90UB913Q-Q1 , DS90UB914Q-Q1 Hello,
I want to transmit data from a FPGA board to external device board (distance <=15m). On the device board…
Other Parts Discussed in Thread: DS15BA101 Hi,
I have a queastion about DS15BA101.
When DS1515BA101 is powered down, is the device possible to input clock?
However,I hope output clock is off at that time.
I would like to continue putting input clock regardless…
Other Parts Discussed in Thread: DS15BA101 Please advise me on interface between DS92LV1021 and DS15BA101.
Can the LVDS output of DS92LV1021 be DC coupled to the differential input of DS15BA101?
The DS15BA101 datasheet specifies the input common mode …
Other Parts Discussed in Thread: DS15EA101 , DS15BA101 , DS30BA101 Hi,
Our application requires a 250 Mbps link onto 75 ohm co-ax and 100 ohm cat-5e transmission lines through a rotating joint. The loss through the rotating joint requires more than the standard…
Other Parts Discussed in Thread: DS92LX1621 , DS15EA101 , DS15BA101 Why are the SerDes ICs DS92LX1621/22 not capable of driving 100m TP cable as the Cable Extender Chipset DS15BA101, DS15EA101?
What is the main function incorporated in the Cable Extender…
Part Number: DS15EA101 Other Parts Discussed in Thread: DS15BA101 Hi Team,
My customer connects the DS15EA101 with the signal from the CMOS image sensor via AC coupling.
They equalize the DS15EA101 and input it to the FPGA with AC coupling.
Some noise…
Hi Chris,
Yes DS15EA101 is an alternative to the LMH0074.
Sure yes you don't have to use DS15BA101 as transmitter or cable driver. It can work with other drivers as long as it meets electrical spec as DS15BA101.
Regards,, Nasser
Hi Kai,
There are two options:
1). DS15EA101 and DS15BA101: In this case, DS15BA101 is used as transmitter while DS15EA101 is used as receiver. Please below note note links to these parts data sheet:
http://www.ti.com/lit/ds/symlink/ds15ea101.pdf
http…
Part Number: DS15EA101 Other Parts Discussed in Thread: DS15BA101 , LMH0324 , DS30EA101 Hello,
I'm looking for simulation models for DS15BA101/DS15EA101 which i could use to simulate transmission line in hyperlinx. The only models I could find are IBIS…
Part Number: LM5109B Customer is asking for coplanarity data for the LM5109BSD/NOPB device.
This is WSON(NGT) and I found this E2E post which discusses a 16-pin WSON device.
I quote:
It turns out that the values you see ( 0.05mm maximum standoff and 0.08mm…