Hi Kai,
There are two options:
1). DS15EA101 and DS15BA101: In this case, DS15BA101 is used as transmitter while DS15EA101 is used as receiver. Please below note note links to these parts data sheet:
http://www.ti.com/lit/ds/symlink/ds15ea101.pdf
http…
Hi Jack,
At lower speed, normally it is possible to do as you have noted. Please note app note below:
https://www.ti.com/lit/an/slla101/slla101.pdf?ts=1601328806692&ref_url=https%253A%252F%252Fwww.google.com%252F
However, given 1Gbps operation and…
Part Number: DS92LX2121 Other Parts Discussed in Thread: DS15BA101 , DS92LX2122 , , DS15EA101 Hi,
I'm using a cable of 5 meters between the DS92LX2121 and DS92LX2122. Can I use the cable extender chipset DS15BA101 and DS15EA101 to compensate the cable losses…
Part Number: DS15BA101 Other Parts Discussed in Thread: DS15EA101 , My customer use DS15BA101 + DS15EA101, some of DS15EA101 " LOS(PIN15) " will be fail.
customer provide DS15BA101 input/ output signal
- Please you kindly help review circuit is OK…
Nasser, we have had good results with the DS15EA101 device. Do you have details of how the DS15EA101 is different than the LMH0074? Do they have different input stages or internal termination?
Thank you
Part Number: TLK1221 Other Parts Discussed in Thread: DS15BA101 , DS25BR120 , DS15EA101 , DS25BR110 Dear all:
I will used two TLK1221 transmit signal between two board. Can TLK1221 transmit 5-10 meters distance with RX/TX ?
Can you help check the pull…
Hi Dave,
I responded to your earlier question regarding DS15EA101. DS15EA101 and DS15BA101 have the same thermal characteristics and therefor DS15BA101 functionality at TJ = 127 deg C cannot be assured.
Regards,,nasser
Part Number: DS15BA101 Other Parts Discussed in Thread: DS15EA101 Dear,
I would like to have a confirmation that I can use the DS15BA101 buffer to drive 25MHz and 80MHz LVDS clocks to a 50 Ohm coaxial cable that could be 2m to 10m long.
Could you also…
Part Number: DS25BR440 Other Parts Discussed in Thread: SN65DSI85 , , DS15EA101 , DS25BR110 I have a design using 4 lanes of LVDS data at 900Mhz, along with an LVDS clock of 148.5Mhz. This output is coming from the TI SN65DSI85 DSI to LVDS converter. On…
Part Number: DS25BR440 Other Parts Discussed in Thread: DS15EA101 , DS15BA101 Hello,
My customer want to use copper instead of fiber to transmit 300MHz signal through 20M line. DS25BR440 may be used for copper cable Driving and Equalization. Below is my…