Part Number: DS125BR820 Other Parts Discussed in Thread: DS160PR410 Hello team,
I have question on (1) DS125BR820 and (2) DS160PR410.
In case input pins(such INA_0+/INA_0-, RX0P/RX0N) are open, what state will be seen on output pins(such OUTA_0+/OUTA_0…
Part Number: DS160PR410 Other Parts Discussed in Thread: USB2ANY Hi Team,
Is there any special programming cable that is needed to program the device via I²c?
Best regards.
Part Number: DS160PR410 Hello,
Can DS160PR410 get out of the Receiver Detection state of LTSSM without a termination resistor at a receiving device connected after the DS160PR410 if the RXDET is in the L3 state? I'm referring to the Table 3 of the DS160PR410…
Part Number: DS160PR410 Team,
For PCIe Gen 4, where is the document or app note describing in detailed the use of VOD and GAIN,
The only thing I see recommended in the docs is,
"For operation in Gen 4.0 and Gen 3.0 links, the DS160PR410 transmit outputs…
Part Number: DS160PR410 Hi TI E2E,
Two questions related to the DS160PR410:
1) How should unused PCIe inputs on the DS160PR410 be handled? Left floating? Connected to ground? Connected some other way?
2) Is an IBIS-AMI model available for this IC?
Sincerely…
Part Number: DS160PR410 It happens during PCIe detection stage.
AC cap is placed between RC and RX pin of DS160PR410.
I see/ don't see RX_detection ramping slope depends on different EP is connected on TX side of DS160PR410.
Is Termination on RX side…
Part Number: DS125BR111 Other Parts Discussed in Thread: DS160PR410 Hi TI E2E,
Do either the DS125BR111 or the DS160PR410 offer a PCIe pass-through mode whereby the the PCIe signals are passed through the IC without any signal processing. If so, how is…
Part Number: DS160PR410 Hi team,
customer configure DS160PR410 as DP redriver (DP-2k,4k). The configuration is RX_DET pull up through 59kohm,PWDN pull down to GND through 4.7kohm, ENSMB pull down to GND through 1kohm, EQ1 and EQ0 pull down to GND through…
Part Number: DS160PR410 Other Parts Discussed in Thread: DS160PR412 Hi There
We use DS 160 PR 410 in our system , and we check power ripple now .
We use switching power to be DS 160 PR 410 power source .
And we find datasheet only recommended operating conditions .
Does it have a max ripple…