Part Number: DS160PT801 We intend to mount DS160PT801 on the backplane. Both Root Complex and Endpoint have local 100 MHz oscillators on their own boards, and these reference clocks are not brought out to the backplane.
For SRNS (Separate Reference…
Part Number: DS160PT801 1. USE DS160PT801, The following is our application topology. Please help evaluate whether the link risk of redriver placed on Riser2 is controllable. Topology description: Before the redriver, it passes through a 4-level connector…
Part Number: DS160PT801 Other Parts Discussed in Thread: USB2ANY Hi, I designed the circuit using the DS160PT801 Retimer, and I want to watch the tuning and eye diagram using a dedicated tool.
I put pin header(3pin) on the communication line dedicated…
Part Number: DS160PT801 Other Parts Discussed in Thread: USB2ANY Hello, here is the topology of our system: RC is a PC, and EP is our FPGA device.
The EEPROM image is programmed with the DS160PT801.hex file provided on the official website. Link establishment…
Part Number: DS160PT801 Hi TI team,
I am currently working on the DS160PT801 PCIe retimer and have a few questions regarding configuration using SINCON .
1. EEPROM Programming via SINCON
I am able to use SINCON to modify the device registers successfully…
Part Number: DS160PT801 Hi,
We are using the DS160PT801 in our design and require the complete datasheet as part of our project requirements. Could you please help us obtain it at the earliest?
Thank you.
Part Number: DS160PT801 Is there a more detailed datasheet for the DS160PT801 product? The current datasheet does not show pin assignments, electrical specifications, or power consumption details.
Part Number: DS160PT801 Hello
we are using only x2 Lane of the DS160PT801 Retimer in our design and we are are not able to write into the SRIS_EN Register. reading the device ID work find but it's also not possible to have a link Training with PCIe…
Part Number: DS160PT801 Hi, I'm Minkyu Cho.
I have a question for debugging AER issue.
Current configuration is as below.
Root Complex (CPU) <-> PCIe Connector <-> Retimer <-> PCIe Connector <-> End Point.
But There are Corectable errors on CPU…