Part Number: DS160PT801 Hi
Please suggest suitable products, the customer's application is to combine 2 PCIe x4 from PCH into one PCIe x8 for PCIE SLOT.
Part Number: DS160PT801 Hi Support Team.
Please tell me the following information of XIO2001IZAJ.
・ Copper pad diameter(mm)
・ Copper pad thickness(mm)
・ Solder mask openting diameter(mm)
・ Solder mask openting thickness(mm)
↓Reference diagram
Thanks…
Part Number: DS160PT801
Hi
Could you help suggest similar products to replace PS8925
PS8925 - PCI Express® Gen 4 16Gbps 4-Lane Retimer - Parade Technologies, Ltd.
Part Number: DS160PT801 Hi Sir,
May I have some questions about DS160PT801?
customer wants to use DS160PT801 on extended able of PCIe4.
1. How many dB that DS160PT801 can recover?
2. how to set the dB setting? need MCU or can be set by H/W(resistors)? …
Part Number: DS160PT801 It looks like the latest version of the datasheet depicts the DS160PT801 must use the same refclk as the root complex. Is that correct? I was hoping to use this part with an optical PCIe interface that did NOT pass the refclk through…
Part Number: DS160PT801 Other Parts Discussed in Thread: USB2ANY Hi, I want to connect this retimer using usb2any. I could not find add on files for sigcon architect. Could someone help me by providing these files please?
BR, Ross