Part Number: DS16EV5110A Hi team,
One of our customers has the following questions
As shown in the figure, the pull-up resistance of 8 signal lines output by DVI is 50 Ω according to the datasheet. As the project requires me to change these 8 resistors…
Part Number: DS16EV5110A We have an extremely dense board design to which we are adding a DS16EV5110A. with severe trace routing constraints and have the following 2 questions:
Q1: Can the data pairs (D0 / D1 / D2) be swapped among the DS16EV5110A's…
Part Number: DS16EV5110A Dear Support,
I am at the design in of the DS16EV5110A for our ruggedized Monitors.
In the Datasheet the resolution is described with max 1080p and 8/10/12 bit color depth.
Are this 12 bit color depth per channel (RGB) or…
Part Number: DS16EV5110A Other Parts Discussed in Thread: DS16EV5110 Dear Sir/Madam
We’re using DS16EV5110ASQ/NOPB in our project, DS16EV5110ASQ/NOPB and was facing some error. Our HDMI output (the monitor) cannot get signal and could not display anything…
Part Number: DS16EV5110A Other Parts Discussed in Thread: DS16EV5110 Hi
My customers need the following functions, use CAT5 signal to connect HOST and Display terminals (HDMI to CAT5 and CAT5 to HDMI) 1. Is there a schematic diagram or information?
Part Number: DS16EV5110A Dears
My customer have used this chip in a condition with only 1.7m cable, and the source eye diagram is very good, but with our device have 14dB boost, the eye become worse, so want your help to double confirm the suggest setting…
Hi Frank,
DS16EV5110A is rated at 2.25Gbps per lane.
In you post, you noted 60 frames. It is important to specify the video resolution and how many bits per pixel. As long as each lane is limited to 2.25Gbps, DS16EV5110 can be used for this application…
Part Number: DS16EV5110A Other Parts Discussed in Thread: DS16EV5110 Greeting, dear colleauges! I have a question for you.
I need to increase cable lenght using IC DS16EV5110A or another IC if you recommend. In this way, i need to use IC in next configuration…
Part Number: DS16EV5110A Hello, TI!
I have a design where the equalizer DS16EV5110A is connected to the SMBus and I control the individual gain of TMDS pair using a microcontroller. The datasheet for the equalizer indicates that for the clock pair…