Part Number: DS16F95QML-SP Tool/software: Hi TI,
We are using this part in a space application.
Can you please confirm that pins 8 & 9 of this 10-Lead Flatpack Package are not connected internally.
We will tie these used pins to ground, please confirm…
Part Number: DS16F95QML-SP Tool/software: Can you tell me the materials used in DS16F95WFQMLV? I need to calculate the thermal resistance through the leads
Part Number: DS16F95QML Tool/software: After reading the datasheet and looking at figures 10&11 it is unclear to me if the common mode / single ended voltage outputs levels are 3V or 5V. My intent is to connect this to an MC/SOC which is 3.3V with a…
Part Number: DS16F95QML-SP Other Parts Discussed in Thread: DS26F32MQML-SP ,
Tool/software:
Hi expert,
My customer intend to use DS16F95QML-SP & DS26F32MQML-SP in LCCC package. These options show on the datasheet.
But customer found the link in the…
Part Number: DS16F95QML-SP Hello Team,
Posting on behalf of my customer:
I am searching for additional packaging information for PN: " DS16F95WFQMLV " I can see on the datasheet that it's a Ceramic Flatpack, but in the dimension section, it's states …
Part Number: DS16F95QML Other Parts Discussed in Thread: DS26C31MQML , DS16F95 , DS26LV31QML Dear design support team.
I am confusing RS485 interface polarity.
According to TIA-485-A, when VA - VB is positive, the logic value is "0". this means…
Part Number: DS16F95QML Hi team,
I want to use the output of this device as input to a 3.3V I/O pin.
The device's maximum input is 3.6V.
I see on the datasheet the minimum output voltage. What is the maximum output so I know I am safely using the…
Part Number: DS16F95QML-SP Hello,
In RS-485 bus architecture if a node (DS16F95QML-SP) is powered off, is there any risk about the component whether it can be damaged or not due to other powered nodes in the bus? And also, is there any possibility that…
Part Number: DS16F95QML
Is there a specification for the minimum or maximum input rise time of this device, for both the single ended and differential inputs? Looks like only the output transition time is specified in the datasheet.
I also see that the…