Part Number: DS250DF230 Other Parts Discussed in Thread: DS125DF111 , DS110DF111 , DS125DF410 , DS110DF410 , , TLK10002 Hello,
My customer is looking for a replacement product for the ADN2905ACPZ.
Can you please recommend a suitable TI product ?
Thank you…
Hi Drew-san,
Drew Miller1 said: About how much insertion loss is there between the source TX and the retimer RX?
->About 0.5dB.
Drew Miller1 said: Also what is the source TX amplitude?
->350mVpp~850mVpp.
Best Regards,
Nishie
Part Number: DS250DF230 Other Parts Discussed in Thread: DS250DF810 Hi Team,
For the DS250DF230ZLST and DS250DF810ABVT, customer wants to config 12.5G. Would you please share this config guide line? When switching between 9.8G and 12.5G, is it necessary…
Part Number: DS250DF230 Hi,
Does the DS250DF230 support the following Ethernet transmission speeds?
・1000BASE-T (1000Mbps)
・2.5GBASE-T (2.5Gbps)
・5GBASE-T (5Gbps)
・10GBASE-LX (10Gbps)
・10GBASE-T (10Gbps)
Best Regards,
Nishie
Part Number: DS250DF230 Hi,
Our customer operates under the following conditions.
1. Is there any guarantee that it will work under these conditions?
・Data Rate Range = 2.4756Gbps
・Frequency = 25MHz
・Register Address = Setting
0x09 = 0x04,
0x18 = 0x10…
Part Number: DS250DF230
Hi Team, I installed Sigcon Architect 3.0.0.10 from the following site. https://www.ti.com/tool/SIGCONARCHITECT Then, I executed the following file however it seems the profile file doesn't support Sigcon Architect 3.0.0.10. ↓ …
Part Number: DS250DF230 Hi Team,
we plan to use EEPROM with DS250DF230, and could you please help on below questions?
1. Regarding the capacity of EEPROM, is it enough to use EEPROM in 256x8bit format? 2. Can EEPROM use EEPROM with address configuration…
Part Number: DS250DF230 Hi,
The customer wants to combine an MSP430F5419AIPZR (master) with a DS250DF230ZLSR (slave) for I2C communication. From the thread below, we can read Clock low period (min) = 1.3 us (400kHz class).
https://e2e.ti.com/support/interface…