Part Number: DS250DF230 Hi Could you please help to answer my question, thank you very much!
Q1: The software version is α version or β version? some register is only β version active in DS depiction
Q2:if need configure the CTLE Boost…
Part Number: DS250DF230 Hi Team, My customer designed their board and is evaluating DS250DF230 (Front-Port Ingress, Module-to-Host). He confirmed CDR Lock (Channel Register Reg0x02=0xD8) however subsequent stage BERT shows "Sync-Loss" in this case.…
Part Number: DS250DF230 Other Parts Discussed in Thread: DS280DF810 Dear TI Design Support Team:
Can you please provide us authorization to access to the DS250DF230 Programmer's Guide(SNLU182)?
Thank you
Sean
Part Number: DS250DF230 Hi All,
Is there a difference between DS250DF230ZLS and PD250DF230ZLS? I would like to confirm the following description in the past Rev. data sheet.
Best Regards, Ishiwata
Part Number: DS250DF230 Other Parts Discussed in Thread: LMK04828 , Hi Team,
I have some questions about retimer. Could you please help me on that?
1. I have two SFP28 SIP optical ports on the boards and the trace between SIP and ASIC are difference between…
Part Number: DS250DF230 Hello, TEAM.
Our customer would like to use the 2x2 Cross-Point and know about setting of register.
How do we set the 2x2 crosspoint? Does it register Channel A and Channel B alternately, or register at the same time where it needs…
Part Number: DS250DF230 Hi Team,
Could you please help to check what does this comment mean:
(2) The input and output negative-voltage rating may be exceeded if the input and output current ratings are observed.
I want to known if this requirement relax…
Part Number: DS250DF230
Hi. I have a question.
If I want to invert the signal, the bit to change the setting are
Add : 0x3D[6], 0x3E[6], 0x3F[6]
Bit name : FIR_C0_SGN, FIR_CN1_SGN, FIR_CP1_SGN
Is the above correct? Also, please tell me how to change…
Other Parts Discussed in Thread: DS250DF230 Component number: DS250DF230
Hello TEAM.
When I configure the DS250DF230 chip according to the programming manual, the Configuration is as follows:
Channel A->A works, channel A->B does not. When I configure…
Part Number: DS250DF230 Hi ,
Can someone provide IBIS-AMI model for this retimer,
I have query that these AMI details are with in ibis extension file or these AMI files are different.