Part Number: DS250DF810EVM Hello,
I'm reaching out regarding a DS250DF810EVM evaluation board our company recently purchased. We would like to request all available documentation for this board.
At minimum, we require the board schematic, but any…
Part Number: DS250DF810EVM Other Parts Discussed in Thread: DS250DF810 Hello,
The customer is using DS250DF810EVM and has installed SIGCONARCHITE3-WRTE software. Then download the SIGCONARCHITECT-RETIMER-PROFILES installation package. But the DS250DF810EVM…
Part Number: DS250DF810EVM Other Parts Discussed in Thread: SIGCONARCHITECT
Would like to use this DS250DF810EVM with SigconArchitect GUI with wRTE V2.0.0.8 but come with LabVIEW issue.
Which version of LabVIEW I shall install? Can use community version…
Part Number: DS250DF810EVM Hi TI expert
I would like to control 16 unit of DS250DF810EVM in 1 pc, any advise?
For testing the number unit of qsfp-dd active cable
Best regards,
Thomas
Hi,
The DS250DF810 cross-point block is located before the CDR, so its configuration is not affected by it. However by default the retimer channel output is muted when CDR is not locked.
Cordially,
Rodrigo Natal
HSSC Applications Engineer
Part Number: DS250DF810EVM Hi gent.,
May I know if the DF810EVM has soldered 1x8 MXP connector? Also, which cable is recommended here if we run it at 25Gbps. thanks.
Steven
Other Parts Discussed in Thread: DS250DF810EVM Would like to know below setting is workable or not
DS250DF810EVM (Tx) > DUT > DS250DF810EVM (Rx)
Without using any signal generator
To measure eye diagram.
Total repower then
I get a signal detect on Ch0, No output because there is no lock.
Check that x09 is 0's on both channels
Set ch0 to 1E to x09. the 09 is a default, I have tried all 0's truns on ch0
Ch1 1E to x09 no output because there is no…