Part Number: DS25BR110 Other Parts Discussed in Thread: DS25BR120 Hello,
is it possible to provide an equivalent input and output schematic for the LVDS Buffer DS25BR110 and DS25BR120? In the data sheet only a block diagram is given. To analyse the behaviour…
Part Number: SN65LVDT100 Other Parts Discussed in Thread: DS25BR120 , DS25BR100 , DS25BR150 , DS25BR110 , Hi, Staff
I'm transmitting it using LVDS as an LCD panel output, but the image is not displayed with the 5m cable. However, since it is visible when…
As shown above, any standard LVDS transmitter will be able to handle at least 10 m. LVDS buffers with pre-emphasis/equalization like the DS25BR120/DS25BR110 can handle some tens of m.
What distances do you actually require?
Larger distances (up to about…
Part Number: DS25BR110 Other Parts Discussed in Thread: DS25CP102 , DS64BR111 Hi,
I'm planning to use a DS25BR110 as input stage on a board, to handle a 2.3Gbit/s link.
In case of input connector disconnection, the IN+/IN- inputs would be left floating…
Hi Marioin,
1. Yes, our device would pass on any periodic or other deterministic jitter not associated with attenuation of the signal.
2. Yes, the signal looks good. The open eye is approximately +/- 130mV in amplitude. This leaves a 30mV margin to our…
Part Number: DS25BR110 Hi Team,
Can you please help with finding a device for Camera link repeater with at least 500Mbps and part to part skew no more than 200ps?
I want to use DS25BR110 LVDS Buffer with Receive Equalization.
The device have 2 pin of…