I'm not sure what the actual problem is. It would be helpful to check the waveforms at the receiver with an oscilloscope.
Anyway, a buffer like the SN65LVDT100 or DS25BR150 might help. But if the cable is too lossy, a transmitter with pre-emphasis…
Part Number: DS25BR120 Hello,
I'm looking for someone to identify the transmission characteristics of the DS25BR120 component. I will be transmitting a signal across a triax cable approximately 50 Ohms at a length of 125 feet. Essentially, I'm, looking…
As shown above, any standard LVDS transmitter will be able to handle at least 10 m. LVDS buffers with pre-emphasis/equalization like the DS25BR120/DS25BR110 can handle some tens of m.
What distances do you actually require?
Larger distances (up to about…
Part Number: DS25BR120 Other Parts Discussed in Thread: DS25BR110 , Dear Support Team,
we have an application were we use DS25BR120 and the DS25BR110 to drive a 500 MHz LVDS signal over appr. 1.5m external cable between two devices.
The cable is a RJ50 cable…
Part Number: DS25BR120 Other Parts Discussed in Thread: DS25BR110 Hi Team,
I Need the IBIS file With Differ Gain Mode. In Web page available One IBIS file.
I need to Simulate with different Gain option for the PE(gain) selection.
My data Rate 1 Gbps…
Part Number: DS25BR120 Hi all Would you mind if we ask DS25BR120? How much is ICC(supply current) in case of PE0=1 and PE1? Our customer would like to know maximum current consumption. There is the description "Figure 13. Power Supply Current as a Function…
Part Number: DS25BR120 Hello Team,
I have a customer with the below question that I was hoping to get an answer for.
Currently the customer's design is using a 100 MHz clock on the IN+ and a 0 volt signal on the IN-. When looking at the output in this…
Hi Gary,
Here are some viable options for SGMII:
DS25BR100
DS25BR110
DS25BR120
DS64BR111
DS64BR401
The DS64BR401 may be preferable due to higher channel count.
Thank you,
Evan
Part Number: DS25BR120 Hi
My customer request me IBIS AMI model or HSPICE model of DS25BR120.
If you have model, please let me know.
Customer application is mobile backhaul.
Best Regards
Koji Hori
Part Number: DS25BR100 Other Parts Discussed in Thread: DS25BR120 , , DS25BR110 , DS25BR150 Hi team,
My customer wants to know the Air Gap Discharge Protection spec of below device. The customer wants ±8kV as the spec. If you have the spec, please let…