Part Number: DS25BR150 To mantain a protective buffer between a backplane connector and an FPGA using DS958.pdf to communicate, the DS25BR150 3.125 Gbps LVDS Buffer is almost a perfect fit. Unfortunately, the IC's maximum output common-mode voltage (1…
Part Number: DS25BR150 Tool/software: Hi Kindly Suggest an Alternate Part Number either with same or different Package for P/N: DS25BR150TSD/NOPB with Temperature Rating of -40 to +125 or -40 to +105 as we require to use the same rated device as per our…
Part Number: DS25BR150 Tool/software: Could you please provide us with the CTE values for the subject part number.
We would appreciate it if you could provide the CTE values in ppm/°C or ppm/°F, as well as the temperature range over which the values…
Part Number: DS25BR150 Tool/software: Hello TI Support Representative,
I'm looking to redrive an LVDS/M-LVDS clock signal that is coming from another board/source into an IC that has strict input slew rate requirements.
I was wondering if the DS25BR150…
Part Number: DS25BR150 Other Parts Discussed in Thread: DS25BR110 Hi,
Good Day.
I actually use DS25BR150, but I would like to use DS25BR110. On my board, pins 1 and 4 are NC and I would like to know if it is a problem with the DS25BR110 because for…
Part Number: DS25BR150 I want to use DS25BR150 LVDS BUFFER on my design.
I would like to know if the input is not connected to the device what should be seen on the output of the device?
Is it supports LVDS Failsafe?
Part Number: DS25BR150 Other Parts Discussed in Thread: DS25CP104A Hi team,
May I have eye mask for SI SIM with LVDS like below figure?
Best regards,
Shunsuke Yamamoto
Part Number: DS25BR150 Other Parts Discussed in Thread: TLV3801 , , DS25CP152 Hello,
We're using TLV3801 https://www.ti.com/lit/ds/symlink/tlv3801.pdf in our application and we're looking to split its LVDS output such that one goes to FPGA and the other…
Part Number: DS25BR150 Hi ti team,
I try to use DS25BR150 to convert MIPI CSI-2 signals to LVDS on the FPGA without native MIPI D-PHY IO support. For HS of MIPI CSI-2, it meets DS25BR150's datasheet. For LP of MIPI CSI-2, with its 1.2V swing, I am npt…
Part Number: DS25BR150 Hi Team,
Good day. I am posting this in behalf of our cusotmer. We have a question about DS25BR150 3.125Gbps LVDS Buffer. On page one of the datasheet, there is a cable to the input of the DS25BR150. What would be the maximum…