Part Number: DS25BR400 Other Parts Discussed in Thread: DS25CP104A
Hello, we are going to create a design based on the DS25BR400TSQ and FPGA, but we do not fully understand the compatibility of the interfaces, in particular:
1 ) Is it necessary to…
Part Number: DS25BR400 Other Parts Discussed in Thread: DS25CP104A HI,
I would like to use DS25BR400TSQ device. and would like to make IS simulations on it.
Can someone consult about the IBIS model? I'll be thankful for receiving it.
Thanks…
Part Number: DS25BR400 Hi dears,
The DS25BR400 is a quad 250 Mbps – 2.5 Gbps CML transceiver, I would just like to know if that means the maximum data rate is 2.5Gbps per channel and the total data rate could get up to 10Gbps. The customer want to use…
Part Number: DS42BR400 Other Parts Discussed in Thread: DS25BR400 Tool/software: Hi E2E,
We are designing a screen display by using CML transceiver DS42BR400.
During the test, We found that the DS42BR400 surface temperature was to hot and the COF…
Part Number: DS15BR400 Other Parts Discussed in Thread: DS25BR400 , DS15BR401 ,
Hi Nasser,
DO we need 100 ohm resistors at the input as shown in the document given in the link below?
https://www.ti.com/lit/ug/snlu010/snlu010.pdf?ts=1696534591539&ref_url…
I've made a typo: "We are interested in the DS25BR400 because the end product requires four independent 1.25 Gbps links and we would like to use a single chip solution instead of 4x DS25BR100 ."
It was supposed to be DS25BR440 and not DS25BR400, sorry…
Hi Gregory,
The DS25BR400 is not compatible with signals down to DC. The inputs are capacitively coupled internally so the external voltage bias will not translate to the device and produce a stable output state.
Regards,
Lee
Part Number: DS25BR440 Other Parts Discussed in Thread: TINA-TI , DS25BR400 Tool/software: TINA-TI or Spice Models Hi we need closer simulation model for the following parts:
DS25BR400, DS12BR400
It seems that Standard IBIS modeling does not support…
Hi Richard,
Thank you for the follow-up responses. I would also suggest to look into DS25BR400 or similar CML devices. This device is capable of 100mV-1560mV input voltage levels at the 2.0 Gbps datarate.
Is the block diagram presented in the initial…
Part Number: DS25BR440 Other Parts Discussed in Thread: DS25BR100EVK , DS25BR400 , DS25CP102 Hi,
I have two things I would like to confirm.
#1
The operation above recommended operating temperature
My client basically plans to use it in an…