Hi Kawai,
The DS25CP104A control pins Sxx/ADDRx/SCL/SDA do not have internal resistors to set levels. The customer should use external resistors to apply either H or L levels to the pins.
Regards,
Lee
Hi Kawai-san,
[Q1] Is SmartPWDN circuitry active in pin configuration mode ? I could only find the SmartPWDN description in the paragraph of register settings, SMBus Mode.
[A1]: The SmartPWDN circuitry or functionality is only available in SMBus mode…
Hi Kawai-san,
The input capacitance of the DS25CP104A/114 is not on the datasheet, but all device parameters for SMBus communication are designed to comply with SMBus 2.0 specifications. Therefore, input capacitance is 10 pF maximum:
Thanks,
…
Other Parts Discussed in Thread: DS25CP104A Hi,
My customer uses DS25CP104A device just for one ch signalling due to some reason.
(Use IN0+/- to OUT0+/- only)
For this case, how should we do for some unused pins?
1: S11/S10 for OUT1, S21/S20 for…
Part Number: DS25CP102Q-Q1 Other Parts Discussed in Thread: DS25CP104A Tool/software: the IBIS-AMI model of the DS25CP104A doesn't work (see the error report below).
The IBIS model cannot load the AMI library. ADS Keysight 2024 update 2 is using for…
Part Number: DS25CP102Q-Q1 Other Parts Discussed in Thread: DS25CP102 , DS25CP104A Tool/software: Dear Team,
We're facing challenge while assigning IBIS model of DS25CP102Q-Q1 in Ansys SIWave. Requesting your help.
Error is as below
*Global - Messages…
Part Number: DS25BR100 Other Parts Discussed in Thread: DS25CP104A , DS25BR120 , DS25CP102 , DS25BR110 , SN65LVDS31-33EVM Tool/software: Dear All,
I'm looking for the most suitable LVDS buffer/repeater/re-driver for the application below.
Three SPI…
Part Number: LMH0397 Other Parts Discussed in Thread: DS25CP104A In the LMH0397, are the OUT0+/- pins tri-stateable? I only have one diff pair available for SDI in or out to my host board, so I want to know if the OUT0+/- pins can be bussed together with…
Part Number: DS25BR150 Other Parts Discussed in Thread: DS25CP104A Hi team,
May I have eye mask for SI SIM with LVDS like below figure?
Best regards,
Shunsuke Yamamoto
Part Number: DS25CP102 Other Parts Discussed in Thread: SN65MLVD206 , DS25CP104A Tool/software: Dear Team,
I am currently facing an issue when attempting to configure the ds25cp102.ibs file within the ADS simulation software.
Specifically, when…