Part Number: DS30EA101 Other Parts Discussed in Thread: DS30BA101 , LMH0394 , LMH0302 Hi TIer
Could you help me explain the compensation capabilities based on different rates of DS30EA101?
I just find a value in 3.125Gbps situation. But it must be used with…
Part Number: DRIVECABLE04EVK Other Parts Discussed in Thread: DS30EA101 , DS30BA101 Hi Experts,
Good day. Seeking your assistance on this query:
Customer is designing a LVDS transmission line (1.5 GBps, for max 20 meters length) using the chipset composed…
Part Number: DS30EA101 Other Parts Discussed in Thread: DS30BA101 , Hello. I use a pair of ds30ba101 and ds30ea101 devices through 5-10m of CAT6A cable. 120MHz clock signal is transmitted on this channel. At temperatures below -10 degrees Celsius, 100ns…
Part Number: DS30EA101 Other Parts Discussed in Thread: DS110DF410 , I have a customer who needs assistance with the DS30EA101 and DS110DF410 adaptive equalizers, used in a system transmitting data through a cable at bit rates around 2.5 Gbps.
For these…
Part Number: DS30EA101 Hello,
We are experiencing an LOS detection on the DS30EA101 when it appears there is still a high-integrity 2.6GHz signal being received; meaning a good eye-pattern is observed on an oscilloscope, and the amplitude of the signal…
Part Number: DS30EA101 Other Parts Discussed in Thread: DS30BA101 , The IBIS model provided on ti.com for this part has a Vdiff parameter of 2.5V. For a device that is capable of picking up signal through a cable path with 50dB attenuation and a source…
Part Number: DS15EA101 Other Parts Discussed in Thread: DS30EA101 , LMH0324 , DS30BA101 , LMH0302 , TEST2 , LMH1219EVM , LMH1219 Tool/software: Hi Team,
I am looking for a simulation model of the DS15EA101 or DS30EA101 that I can use to simulate transmission…
Hi Krupanand,
One option is the https://www.ti.com/product/DS30EA101DS30EA101. It has a speed greater than 3 Gbps, specifies the required outputs in the datasheet, and is an equalizer. Does this meet your application requirements and do you have any more…
Part Number: DS30EA101 On the DS30EA101SQE, pin 8 is stated as VEE.
The question is whether it is OK to leave pin 8 open.
Is pin 8 really VEE (and connected internally to the other VEE pins) or it actually is some control input that must be grounded? …
Part Number: DS30BA101 Other Parts Discussed in Thread: DS30EA101 Hello, I would like to use the DS30BA101 and DS30EA101 to transmit and receive 8b/10b encoded data over 50 ohm coaxial cable. The cable is about 1 meters long and data rate is 3.125Gbps. …