Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Hi Kai,
There are two options:
1). DS15EA101 and DS15BA101: In this case, DS15BA101 is used as transmitter while DS15EA101 is used as receiver. Please below note note links to these parts data sheet:
http://www.ti.com/lit/ds/symlink/ds15ea101.pdf
http…
Greetings,
DS30BA101 and DS30EA101 could be used in this application. However, these devices have not been characterized at 20Mbps and thus data sheet specs cannot be guaranteed. Having said these, these device can operate at this low rates.
Regards…
Hi Min,
Please take a look at DS30BA101 and DS30EA101 driver and equalizer. However, we do not have a quad driver and equalizer in one pkg.
Also, i am not sure about your cable insertion loss. DS30EA101 have about 10-15dB gain at about 150MHz(Nyquist…
Hi Nasser-san,
Thanks for your support.
I understood that DS15BA101 and DS15EA101 does not have models for high speed signal path simulation. I believe DS30BA101 and DS30EA101 have the same situation.
Best Regards,
Kawai
Hi Piet,
We do not have an IBIS model for the DS15EA101. The DS30EA101 is an updated device which has an IBIS model available.
See the Featured Tools and Software section of the product folder link below.
http://www.ti.com/product/DS30EA101
Regards,
…
Part Number: LMH0344 Other Parts Discussed in Thread: DS30EA101 Hello team,
We are using LMH0344SQ/NOPB for SDI equalizer circuit in our design.
What would be the preferrable termination for differential inputs(SDI,SDI/) , whether i can use 100ohm or 75…
Hi Andoon,
1). Please note LMH0307 is a 3.3V cable driver so we should use 3.3V for R31, R32, R35, and R36.
2). Please take out return loss network(5.6nH, 24.9-ohm, L1, L2, R15, & R16).
3). Please take a look at DS30EA101 and DS30BA101 devices for…
Hi,
Our customer uses DS30EA101 with DS90UB928Q. The DS30EA101 differential output is automatically disabled (to a logic 1) by LOS and EN being tied together when no input signal is present. Therefore ±450mV (Max) continues being applied to DS90UB928Q…