Part Number: DS320PR1601 Hello TI team,
I am currently designing a PCB using the DS320PR1601 and would like to request your assistance to review the layout for potential issues or recommended improvements.
Due to confidentiality, I cannot share the…
Part Number: DS320PR1601 Hi TI support team,
I am using the DS320PR1601 for a PCIe x16 link.
To facilitate a better PCB layout, I would like to swap the RX lanes on the redriver. For example:
PCIE_RX0 → DS320PR1601 RX15
PCIE_RX1 → DS320PR1601…
Part Number: DS320PR1601 Tool/software: Hi, Team
I have the following questions:
In DS320PR1601 datasheet
Pin FJ3 is A_ADDR1_15-8
Pin FF5 is A_ADDR0_15-8
In HSDC111_DS320PR1601-RSC-EVM schematic
Pin FJ3 is A_ADDR0_15-8
Pin FF5 is A_ADDR1_15…
Part Number: DS320PR1601 Is 32 the maximum number of configurations that are allowed by the SigCon Architect Tool when used to configure a DS320PR1601. If so can this be increased or must a design be split into multiple separate chains in order to supports…
Part Number: DS320PR1601 Tool/software: Hi,
I am using DS320PR1601, for our new project.
I am attaching the stack up our board.
I got the DS320PR1601 EVM board details from TI.
Also we referred its layout and stack up file.
We understood that…
Part Number: DS320PR1601 Tool/software: Hi,
in DS320PR1601, READ_EN# signal is used for loading redriver configuration from EEPROM when used in primary mode.
for our application we are using primary mode.
if READ_EN# signal is made low using some…
Part Number: DS320PR1601 Tool/software: Hi,
how is power down pins related to the working of Redriver.
if the endpoint is a ssd, does it mean pd =low means ssd detected at root port?
how is perst and prsnt signal related to pd pins?
Thanks…
Part Number: DS320PR1601 Tool/software: Hi,
I am using DS320PR1601, do we need to copper pour?
if so do we need to copper pour on both sides of tranceiver signals?
how copper pouring ffect pcie gen5 signals
Thanks and Regards,
Shekha …
Part Number: DS320PR1601 Tool/software: Hi,
Can we simulate eye diagram without connecting Redriver based board in SigCon Tool 3.2.
Thanks and Regards,
Shekha Shoukath
Part Number: DS320PR1601 Tool/software: Hi,
kindly tell whether we can use 3 times track width for intra spacing in case of refclk signals for DS320PR1601.
thanks and regards,
Shekha Shoukath