One more thing is that the node for IPU1_0 is not exist on /sys/kernel/debug/remoteproc#.
-------------------------------
root@dra7xx-evm:/sys/kernel/debug/remoteproc# ls -la
drwxr-xr-x 5 root root 0 Jun 11 19:54 .
drwx------ 30 root root 0 Jan…
Part Number: DRA76P
Tool/software: Linux
hi all,
i load visionSDK IPU2 firmware into EMMC IPU2 partition, and i modify the uboot and kernel DTS according:
my use case is create chains on M4 size, if IPU firmware loaded and started success, it…
Hi,Brenda
We enabled the 200Ω discharge path of PMIC(TPS65224) LDO3. However, the power-off test still failed to meet this requirement(It is recommended to discharge a supply group below ~300mV before the next rail in sequence is turned OFF.)
The…
Hi,
Thank you very much for your kindness.
I really appreciate your help.
1: I'd like to send the log.txt.
2: I've met this problem many time (not first time).
We would appreciate if you tell us how to solve this problem.
Best regards…
Hi Shravan,
I have compared the difference in vsdk3.4 and move it to vsdk3.2. The SDKs are similar with a little difference, so I do not apply the difference to my vsdk3.2.
I was browsing the forum recently.I find that the LATE_ATTACH macro is defined…
Part Number: J784S4XEVM Other Parts Discussed in Thread: TDA4VH Tool/software: Hi TI experts, We create custom board for tda4vh, and have problem for load firmware and start dsp core in tda4vh with bellow log for dmesg [ 6.143211] virtio_rpmsg_bus virtio0…
Hi Nicholas :
1.The documents I refer to are attached(J784S4 Single Leo Dual HCPS PDN-3AFGM v0.23b)
J784S4 Single Leo Dual HCPS PDN-3AFGM v0.23b.pdf
2. "EN_3V3_VIO" is the GPIO9 signal of TPS6594133A-Q1.
Please find attached below revised SCH & block diagram that will be released to TI website soon that addresses your questions.
PROC131E2A_SCH.pdf
AM68x SK Edge AI Flex Tulip PDN-6H v0.11.pdf
Hi Sahin,
Thank you so much for your help!
I had updated my rsc_table_dsp.h as you told. now I did not see " bad address..." as before. but I still got some errors. see message below. Do I need to modify dts file as well? or something still missing…
Hi Jeff and Yordan.
I have changed everything that we talked about it, but it has not work still.
reserved-memory {
#address-cells = <2>;
#size-cells = <2>;
ranges;
dsp_common_cma_pool: dsp_common_cma_pool@81f800000 {
compatible = "shared-dma-pool…