Hello,
Thank you for your patience on this. Below are the thermal details:
Result- Theta JA-High K (standard datasheet value)
76.7
Result-Theta JC, top (standard datasheet value)
34.0
Result-Theta JB (standard datasheet value)
35.3
Result- Psi…
Part Number: DS34LV86T The question is basically fully stated in the title, the datasheet did not mention that external termination resistors where required, nor did it mention if termination resistors are included inside the enclosure.
Part Number: DS34LV86T Hello Team,
Good day. My customer is looking for the maximum rated junction temperature for the DS34LV86TM/NOPB can you share this information to us?
Regards,
Renan
Part Number: DS34LV86T Hello Team,
My Customer is looking for the Thermal information of DS34LV86TM. Can you share this information with us?
Regards,
Renan
Part Number: DS34LV86T Hi Team, Our customer would like to know 2 things for DS34LV86T below: 1. Can it be used with 5v signalling (differential 5v (RS-422)). 2. If it is used with 5v signalling, and fail safe resistors are used, are they pulled to +5v and…
Part Number: DS34LV86T
Hi E2E,
Good day.
Our customer is looking for the thermal Information (Theta Jc, Theta Jb) and Tjmax of DS34LV86TM, DS34LV87TM and SN74LVC16245AZQLR.
We appreciate your support and thank you in advance for your help.
Best regards…
Hi Max, yes it is closed. There was another component on the board that was the source of the issue.
Thank you for the support. Sorry for the goose chase.
Russell
Part Number: DS34LV86T Hello community,
I'm posting here as I'm unsure of where else to post this question for these two devices.
For the two PNs: DS34LV86TM and DS34LV87TM, my team and I are trying to determine if the RoHS replacement with "…
Other Parts Discussed in Thread: DS34LV86T , DS34LV87T , AM26LV31E , AM26LV32E If there are spec & data about the impulse withstand voltage of four products below, please let me know. - DS34LV86T - DS34LV87T - AM26LV31E - AM26LV32E Since I think that…