Hello,
So very sorry about the delay. It normally doesn't take us this long to get this data. I was able to secure a thermal stream today to do the testing.
Temperature
Unit1
Unit2
Unit2
-20C
3.17V @5.13mA
3.17V @5.13mA
3.18V @5.13mA
25C
3…
Part Number: DS34LV87T Tool/software: Hi sir,
Our system uses three DS34LV87T chips to convert the UART signal from single-ended to differential. Currently, we are encountering a problem where the output P exhibits the waveform shown in the image below…
Part Number: DS34LV87T Hello TI,
Our system incorporates a line driver for the transmission of consistent data in the form of differential signals to the other side, where we are encountering data delays at the differential signals (i.e. Output of the…
Part Number: DS34LV87T Hello Team,
I'm posting on behalf of my customer:
I am looking for additional documents related to electrical calculations for the devices DS34LV87TMX/NOPB and DS34LV86TMX/NOPB. It would be really great if we are able to see…
Part Number: DS34LV87T Hi team.
I am estimating the current consumption of the circuit.
Am I correct in recognizing that the maximum total current consumption of DS34LV87T is as follows?
Icc(100uA) + Io(150mA) x 4 outputs = 600.1mA
Also, the above calculation…
Part Number: DS34LV87T Hello Team,
Good day. My customer is looking for the thermal information of DS34LV87TM/NOPB. This is not provided in the datasheet, can you share this data to us?
Regards, Renan
Part Number: DS34LV87T Hello Team,
My Customer is looking for the Thermal information of DS34LV87TM. Can you share this infomration with us?
Regards,
Renan
Other Parts Discussed in Thread: DS34LV87T We are using the TI DS34LV87T as an interface circuit in our system.
We have a failure with driver D2, the other drivers function normally. When powered off, pin 5 (DO2-) is shorted to GND (pin 8). Pin 6 (DO2…
Other Parts Discussed in Thread: DS34LV86T , DS34LV87T , AM26LV31E , AM26LV32E If there are spec & data about the impulse withstand voltage of four products below, please let me know. - DS34LV86T - DS34LV87T - AM26LV31E - AM26LV32E Since I think that…