Part Number: DS560DF810 Hello, For the implementation of the DS560DF810, I want to know if the retimer needs a patch and if yes how to roll it out, as the information in the DS560DFxx0 Programmer’s Guide SNLU294 does not seems complete. In 5.3.4 of the…
Part Number: DS560DF810 Hello TI team,
We are developing an 400G / 100G production-line bit error rate tester (BERT) and are evaluating the DS560DF810 56-Gbps multi-rate retimer for our design.
We already have the DS560DF810 datasheet (SNLS709B) and…
Part Number: DS560DF810 HI,
I am currently working on a design that involves the DS560DF810 component, and I require specific mechanical data to proceed with heatsink mounting considerations. Could you please provide the maximum package compressive…
Part Number: DS560DF810
Hi Team,
We are currently working with the 56G Retimer DS560DF810 (135‑pin fcBGA package) and are looking for the junction‑to‑ambient thermal resistance (RThetaJA) value.
Upon reviewing the datasheet, we noticed that the…
Part Number: DS560DF810 Other Parts Discussed in Thread: DS560DF410 , Hi team,
The program guide for the DS560DF810/DS560DF410 does not contain details for the following macro. Could you please provide them?
LUT Mapping Configuration for DFE 0x4C…
Part Number: DS560DF810 Tool/software: Hi Team,
Currently Nokia is investigating the use from the DS560DF810 Retimer (with crosspoint) in thier application.
They are looking for a solution to switch between two different 50G (output) channels. As…
Part Number: DS560DF810 Tool/software: As previous asked in DS560DF810EVM: loopback test failed can't meet my expectation
Mr. Drew Miller, suggest a topology for us to make the DS560 generate the pattern.
Right now, I have setup the evm board with…
Part Number: DS560DF810 Hi team,
Is there a recommended environment for running the API? For example, would it be possible to use an Arduino as the I²C master and configure it from VBA?
Best regards, Goto
Part Number: DS560DF810 Here is the original text from the manual. My questions are:
1. Does the DS560 not automatically switch to Target mode like the DS280 does?
2. What does the second step in the text below mean? Do I need to configure a register…
Part Number: DS560DF810 Tool/software: Hi,
As far as I see CAL_CLK_OUT is buffered replica of CAL_CLK_IN input.
8 x retimers are planning to be used. I am wondering that if you have a limitation/ recommendation on how many devices can be connected…