Part Number: DS80PCI402 Hello E2E Experts,
I am using two DS80PCI402 devices across two different PCBs. Based on TI's Typical Application, appearing in the datasheet, this configuration seems correct. In my setup, there are three PCBs in total: one…
Part Number: DS80PCI402 Hi Team,
I have a question about the PCIe Gen 3.0 redriver use case. If a redriver Part No: DS80PCI402 is implemented on the motherboard design, is it also necessary to place a redriver on the add-in card? As you can see there…
Part Number: DS80PCI402 Tool/software: Hello,
the datasheet states that even in 2.5 V mode, all 4-level inputs that have a connection to "logic 1" must be connected to VIN (3.3 V).
Is this correct, or can the pull-ups also be connected to 2.5V VDD…
Part Number: DS80PCI402
Dear Technical Support Team,
I am planning to use the DS80PCI402 in a new design and I would like to confirm two technical points.
1. Differential pair swapping within the same channel group
For layout reasons and to better…
Part Number: DS80PCI402 Tool/software: Hello team
If two different devices are set by pin mode and SMBus mode with same configuration , is there a any difference in terms of performance?
Best Regards,
Austin
Part Number: DS80PCI402 Tool/software: Hi, Dear supporter,
I am using DS80PCI402 to boost a 2x PCIe connection. If I using pin mode, set pin state as following, the EP device can be enumberated by host.
ENSMB
1K to GND
EQA…
Part Number: DS80PCI402 Tool/software: Dear Team,
My customer has evaluated the DS80PCI402SQE on their board. They would like to have the Pin-to-Pin short test results of the DS80PCI402SQE. If you have it, please send it to me.
Best Regards,
Koshi…
Part Number: DS80PCI402 Hello, My customer is considering to transmit PCI Gen1 data from FPGA#1 to FPGA#2 via 1m length FR4 PCB trace. Just one DS80PCI402 is good enough to compensate the 1m FR4 PCB trace loss? Or two DS80PCI402s should be cascaded? If…