Part Number: DS80PCI402 Other Parts Discussed in Thread: DS80PCI102 Dear team,
We want to design DS80PCI402 between CPU and two PCIe device(x2 lanes).
Is there any side effect for this application? please share your suggestion with us.
Thanks,
Ben
Part Number: DS80PCI402 Hello, Q1: My customer plans to use DS80PCI402 between PCIe Gen1 host card and PCIe Gen1 slave card. The DS80PCI402 is mounted on either the host card or slave card. At their application the host card and the slave card are hot…
Part Number: DS80PCI402 We are having issues with PCIe communication on a DS80PCI402, driving a VPX card on one side and two in series 1M iPASS cables on the other side. Does this device support any type of S/W app/circuit that allows the received eye…
Part Number: DS80PCI402 Hi team,
My customer is using VID=1.2Vp-p for application
Based on Datasheet, VOD should be 0.8-1.2Vp-p when VID=1.0Vp-p.
What is the VOD SPEC when VID=1.2Vp-p?
Or could we say VOD's SPEC is same as datasheet when VID=1.2Vp-p…
Part Number: DS80PCI402 Hello,
we are facing a power-up issue on a PCIe x4 link between mainboard and (FPGA based) PCIe add-in card where the DS80PCI402 is used as Re-Driver between mainboard slot and card slot (link is not getting established or in x1…
Part Number: DS80PCI402 Hi Team,
Our customer will connect the DS80PCI402 to COM Express module and would like to confirm if the 220nF caps should be added to all input/output pins of the device. According to the customer,
1. the COM Express module includes…
Part Number: DS80PCI402 Other Parts Discussed in Thread: DS50PCI401 , DS125BR401 , Since we have a shortage for this device , do you have a pin to pin replacement ( running at 5Ghs or higher) ?
I used the internal 2.5 volts for now
Part Number: DS80PCI402 Other Parts Discussed in Thread: DS80PCI800 Hi Ti
Can you send the DS80PCI402 software debugging package to us for reference?As shown in the figure below, it is not downloaded from the official website. Thank you
Part Number: DS80PCI402DS80PCI402 datasheet page-8 is described VTX-DIFF-PP (VOD): 0.8V_min to 1.2V_max
I guess that above VOD: 1.0V setting, and variation is ±20%.
Is it correct?
Please let me know about VOD variation in the case of VOD: 1.4V…