Part Number: DS89C21 Tool/software: Hello,
I would like to implement an AC termination for a reduced consumption with an inverted polarization to ensure a low output in case of failure of the input in high impedance or short circuit according to the…
Part Number: DS89C21 Hello!
My name is Oleksii Mitin. I am working in S and Y Industries, Winfield, Ks, USA.
I have a next question.
What difference between DS89C21 and DS89C21TM/NOPB?
What does means TM/TMX/NOPB? I can't find information anywhere…
Part Number: DS89C21 Tool/software: Hi All,
I have a question about the DS89C21.
Could you please tell me the Common-Mode input Voltage Range on the receiver side?
The Absolute Maximum Ratings state Receiver Input Voltage—Vcm, but what is the recommended…
Part Number: DS89C21 Hi,
I am requesting the values for the
1. Junction to Case Thermal Resistance
2. Junction-to-top characterization parameter
-for the DS89C21TMX/NOPB.
These values with assist in our thermal analysis. Thank you.
Best…
Part Number: DS89C21 Tool/software: Hi All
Could you please confirm the circuit diagram for DS89C21? I would like to share the circuit diagram via private message because it is confidential information. Please contact me.
Best Regards, Ishiwata
Part Number: DS89C21 Tool/software: Hi All,
I have a question about the DS89C21.
Could you please tell me the Common-Mode input Voltage Range on the receiver side?
The Absolute Maximum Ratings state Receiver Input Voltage—Vcm, but what is the recommended…
Part Number: DS89C21 Hi team,
I got a question from customer.
"Model: DS89C21TMX NOPB, when debugging, 5 feet were short circuited. The attached circuit diagram is for reference. Please analyze the reason.
Problem: when the elevator runs automatically…
Part Number: DS89C21 Hi All,
I have a question about DS89C21.
If the input terminal (RI / RI *) on the receiver side is not used, can I connect it to GND?
Best Regards, Ishiwata
Part Number: DS89C21 Other Parts Discussed in Thread: DS8921 , Hi,expart.
What is the difference between DS89C21 and DS8921? Is DS89C21 a next-generation product of DS8921?
Best regards. Ryuji
Part Number: DS89C21 Hello
My customer is considering to use the DS89C21TMX.
could you tell us min, typ and max spec for the DS89C21TMX at below condition?
Vcc= +4.85V
Ta = + 25C
best regards,
Kazusa suzuki