Part Number: DS90C402 Hi,
Customer have some confirmation regarding this IC.
- What happens if the ground pin of the DS90C402 is not connected to the ground pin of the corresponding LVDS driver? Not sure about the driver side since it is embedded…
Part Number: DS90C402 Hello,
My customer is requesting for the value of the internal pull up in the input pins of the device.
Appreciate your help.
Regards, Roland
Part Number: DS90C402 Hello Team,
My customer is requesting details below as they make their Failure Mode Effects and Criticality Analysis.
Regarding device DS90C402: 1. On what particular conditions will the device fail? 2. During failure, how will…
Hi Sagar,
Can you clarify what you mean by "energized" and "DC voltage?" If the DS90C402 is powered down and there is an active signal sent to the device, this should not be a problem. However, if there is some kind of large transient going into the…
Other Parts Discussed in Thread: DS90C402 , DS90LV028A Hi,
I cannot find the IBIS model for DS90C402 on webench.ti.com/.../
nor can I find it in the zip file focus.ti.com/.../ti_ibis_models.zip
Can anyone tell me where elese can I find the IBIS…
Hi Samuel,
DS90C402 is also compatible with EIA-644 and electrical spec is compatible with the 3V driver. So you can use DS90C402 as well.
Regards,,nasser
Hi Stefan,
Sorry, I just noticed that you asked a follow-up question in your previous post.
It looks like we don't have any 5V TTL receivers with integrated termination. However, there is the DS90C402, which is a 5V receiver without integrated termination…
Part Number: DS90C401 Other Parts Discussed in Thread: DS90C402 , Hello,
We have a customer who is having issue with both the DS90C401 and DS90C402.
From customer:
"I killed my first driver. Receiver seems OK. I built a driver to receiver prototype…