Part Number: DS90CF386
Hello,
Switching Characteristics are described in the datasheet of "DS90CF386".
Only the characteristics at 85MHz are listed.
Would you tell us the "Switching Characteristics " at 65MHz and 75MHz.
Part Number: DS90CF386 Hi Tech Support Team,
We are working for Video recorder design, which receives Analog HD camera inputs and IP camera inputs.
As part of output we have one digital output using HDMI interface and one analog display through BNC which…
Part Number: DS90CF386 Hi Bryan-san
It is related question from below,
I could not get your answer for #2.
Could you please give me your comment for the #2?
2. According to the specifications "7.1 Overview", the following is stated, so if you set /…
Part Number: DS90CF386 Dear Support Center,
There are four additional questions.
Q1) If the clock frequency is not 85 MHz, will the jitter range be the same as 85 MHz?
For example, 25MHz, 54MHz, 65MHz.
Q2) Does DS90CF386 support Spread Spectrum Clocking…
Part Number: DS90CF386 Hi sir,
We use the DS90CF386 to convert LVDS of NXP iMX6 to RGB888 interface. IMX6 spec: https://www.nxp.com/docs/en/data-sheet/IMX6DQIEC.pdf
The frequency setting of LVDS and PCLK is 80MHz, but the frequency of PxCLK out is 133-136MH…
Part Number: DS90CF386 Dear Support Center,
I am writing to ask about Jitter specification of RxCLKIN-/ +.
The following is described in Note 2 of the data sheet [6.6 Switching Characteristics] of the DS90CF386.
"Receiver skew margin is defined as the…
Part Number: DS90CF386
Hi Expert,
Please tell me about the method of termination for unused pin . Conditions: -There is power supply to the device. ・ Input Low to / PDWN ・ There is no transmitter connection, only the terminal 100Ω connecting each +/- i…
Part Number: DS90CF386 Other Parts Discussed in Thread: TFP410 , SN75LVDS82 , Hello
We are planning to implement a LVDS to DVI Interface. The plan is to prallelise the LVDS signals and send it trough the TFP410.
Now I'm looking for the right device to make…
Part Number: DS90CF386 hi dear supporting team,
for the reference design of CF386, Should customer isolate PLL_GND , LVDS_GND AND VCC_GND through 0 Ohm or ferrite bead? and for RXOUT serial resistor, should they use 50 ohm? tks!
Part Number: DS90CF386 Other Parts Discussed in Thread: DS90C385A Hi,
I'm using DS90CF386. I have some questions about this chip. Could you please help me?
1. The input data of the LVDS to RGB and time sequence is 1:1 or 7:1?
2. The LVDS output voltage…