Hi Lacey,
1. Yes
2. They need to use the SPI CLK as the input clock for the SN65LVDS93A if the frequency is 100MHz.
3. Shielded Cat -5/-6/-7 should be fine.
4. Yes. However, if they're now certain that the frequency is 100MHz then they can consider…
Hello Adrien,
Although there exist parts for going from LVDS -- > Parallel --> DVI, I don't believe we have any Open LDI 24-bit Single Pixel Mode LVDS --> Parallel parts that can support that resolution. A 1920 * 1080 screen (assuming 10% blanking…
Other Parts Discussed in Thread: DS90CF388 , DS90CR484 , DS90CF388A Hello, Could you please let me know the latency of DS90CF388? I would like to know the delay time from input the data to output the data. The input clock is 74.25MHz. Best Regards, Ryuji…
Hi Nao,
Based on your need for 1080p 60 fps, I think you will need to use an RGB-to-OpenLDI converter that is able to operate the correct pixel clock frequency. From my understanding of Jacinto 6 (DRA746), there are 3 LCD outputs that will provide…
Hi,
Thanks for your patience, as we were out on holiday in the U.S. this past week. I do not think this will work with the operating clock frequency you are designing for.
The reason is because of the supported clock frequencies for this chipset…
Hi Umberto,
I looked at the camera datasheet, and from the specifications, it looks like they have an OpenLDI LVDS interface built into the camera:
The LMH0340 uses a different interface than what the THC63LVD104C does, so this device cannot be…
Hi Hong,
There may be a way to implement an LVDS-to-DVI solution with 2 chips, such as with a DS90CF386 or DS90CF388 to convert from OpenLDI LVDS (4 data + 1 clock) to 24-bit LVCMOS. Afterwards, the LVCMOS RGB data can be sent to a TFP410 to convert…
Hi Dave,
We have the following devices support LVDS to RGB.
DS90CR286-Q1
SN65LVDS86A
SN65LVDS96
SN75LVDS82
SN65LVDS94
SN65LVDS822
DS90CF388
and etc
What kind of application do you need LVDS to RGB? If you can provide more information,…
Other Parts Discussed in Thread: SN75LVDS83B , DS90CF388A , SN75LVDS82 , DS90CF388 Hi Everyone,
We are using an Aptina MT9P006 image sensor and plan to serialize the image data with the SN75LVDS83B at 96MHz. The price and compact (bga) size of the SN75LVDS83B…