Part Number: DS90CR218A Hey team,
Our customer is looking for a video converter solution. They need to convert LVDS (oLDI) to either HDMI or to parallel RGB data.
I found the slla559 whitepaper, but the DS90Cxxxx chips referenced there have an operating…
Part Number: DS90CR218A Other Parts Discussed in Thread: LM98620 Hi Sir,
We are looking for Deserializer likes DS90CR218A which is to 3.3V, but we need solution to 1.8V. Using behind LM98620.
Here is LM98620 BU feedback:
"TI has 1.8V LDVS product such as SN65LV302…
Part Number: DS90CR218A Hi team,
My customer considered to use DS90CR218AMTDX/NOPB for decoding LVDS image signal. However, he recently noticed that it only supports 12M~85MHz clock rate whereas he would like to address 85.5MHz in accordance with VESA…
Part Number: TFP410 Other Parts Discussed in Thread: DS90CR216 , DS90CR218A Tool/software: Hello E2E Experts,
Good day.
We are currently looking into the TFP410 to convert the output of a TI DS90CR216 Chip.
According to this application note the DS90CR218A…
Part Number: DS90CR218A Other Parts Discussed in Thread: DS90CR216A , , DS90CR215 Please let me know about calculation for tolerate maximum clock frequency.
Before using DS90CR216A on 36MHz clock.
But latest model is changed 36MHz to 45MHz, DS90CR216A…
Part Number: LM98725 Other Parts Discussed in Thread: DS90CR218A Hi all,
I want to use LM98725 for CIS sensor.
Can LM98725 be used for CIS Sensor?
I want to use STM32H723xx. (MCU)
I want to use LM98725 via PSSI pin (MCU function).
I don't know that How…
Other Parts Discussed in Thread: DS90CR218A , DS90CR217 Hello, We have an application in which we are using a DS90CR217 serializer and a DS90CR218A deserializer to transmit and receive data. This app must be able to operate at two different frequencies,…
Other Parts Discussed in Thread: DS90CR218A , DS90CR217 Hello,
I am using a DS90CR218A / DS90CR217 serdes pair. For a new design I will be using an FPGA to do the serializing. Is the serializer just simply converting 7:1 or is there a synchronizing sequence…
Hi Betty,
The only other device that I see which would come closer to the clock requirements is DS90CR218A at 12MHz. Maybe the customer can check with the display vendor to see if it can be over-clocked to 12MHz?
Regards,
Logan