Part Number: LM98620 Other Parts Discussed in Thread: DS90CR218A
Hi,
In my design used LM98620 + DS90CR218A to get parallel RGB data from adc.
Schematic is followed same as reference design available at LM98620 datasheet (Page no: 59) [R0-R9, G0-G9…
Hi Salim,
There's no issue with using RGB666 data with the TFP410. The unused inputs can just be tied to ground.
Looking at the block diagram in the datasheet of the processor on page 2270, it looks like the frequency range of the LVDS output clock…
Hi Caroline,
Another solution is DS90CR218A(12 to 85MHz).
AN-1538 offers guidance how to interface LVDS to DS90CR218A de -serializer
www.ti.com/.../getliterature.tsp
Regards,
Costin
Hi Sulyn,
We don't have a solution that can support 6.5MHz yet.
Are you considering to use 8 Bit RGB Mode for 320RGB x 240? The fclk is 27MHz.
Also have you looked into DS90CR218A? The min fclk is 12MHz instead of 20MHz.
Most importantly, FPGA usually…
Part Number: DS90CR217 Other Parts Discussed in Thread: DS90CR218A Dear Team,
My customer is facing an issue with the DS90CR217 regarding data transmission.
You can see below the detail of the issue, sent by my customer :
============================…
Hi Mark,
Unfortunately, there does not appear to be a part that meets the exact description of being a drop-in replacement with a 56-pin TSSOP.
The only options for receivers that operate down to 18 MHz or less I notice in the portfolio are the DS90CR218A…
Hi Jamie,
The parts you are using are FPD-Link, where the receiver is designed to strobe on the falling edge.
There is an equivalent Channel LInk part where the receiver strobes on the rising edge. Please take a look at the DS90CR217 (Serializer) and…
Hi,
You can use any generation 1 FPD-Link, Channel Link or Flatlink deserializer with the DS90C185.
This includes the:
DS90CR288A
DS90CR218A
DS90CR286A
DS90CF386
DS90CF366
Most of these 7:1 LVDS deserializer type devices have been incorporated into…
Other Parts Discussed in Thread: LM98620 , LM1117 , DS90CR218A Hi,all
Let me ask you two questions about LM98620.
1)What is the difference between "Continuous Input Current at any pin" and "Continuous Input Package Current" on datasheet_P7…