Hi Tom,
Sorry for the delay in updating the datasheet. I can assure you that the datasheet update request has been submitted and is in progress.
Regards,
Ryan
Part Number: DS90CR485 Is Pin 24 DC balance working in this part, the datasheet Figure 12 is label as GND?
If I connect pin 23 low do I only get data from channels A0P, A0M, A1P, A1M, A2P, A2M and A3P and A3M on rising edge of the clockin? Is the output…
Other Parts Discussed in Thread: DS90CR485 Hi
My customer is using DS90CR485. I think PRE-pin pull-up max voltage is Vcc level from P11 of datasheet. But my customer desgined that pull-up voltage is 3.3V. Because my customer thinks that this pin has…
Other Parts Discussed in Thread: DS90CR485 , DS90CR287 , DS90CR486 Hi
Can use DS90CR485 EVB to connect DS90CR288 to try function?(Due to here have no DS90CR287 EVB)
Best regards,
Bogey
Part Number: DS90CR486 Other Parts Discussed in Thread: DS90CR485 , Hi,
The customer has connected and tested the "transmitter DS90CR485" and "receiver DS90CR486", but the receiver DS90CR486 does not output data. They have confirmed below. ・ RxCLKOUT…
Hi,
The DS90CR486 DC balancing only works if the transmitter (presumably the DS90CR485) is also in DC-balance mode. Otherwise, the serialized bit mapping into the DS90CR486 will not match as expected.
Please provide a schematic of Tx and Rx if possible…
Hi George,
If the HDMI receiver device that you are using outputs different pixels on rising or falling clock strobes, you need a device that support this double pump action(DDR) with a function to support a split out to a dual pixel interface or a…