Part Number: DS90CR486 Other Parts Discussed in Thread: DS90UB948-Q1 Hi,
Is the DS90CR486 compatible with the deserializer DS90UB948-Q1? The Deserializer outputs single OLDI up to 133MHz, but the DS90CR486 has 7 data channels for input with a single…
Part Number: DS90CR486 Other Parts Discussed in Thread: DS90CR485 , Hi,
The customer has connected and tested the "transmitter DS90CR485" and "receiver DS90CR486", but the receiver DS90CR486 does not output data. They have confirmed below. ・ RxCLKOUT…
Hello ,
First thanks for your answer but I do not think I understand it .
this mean I can connect full spec camera link with 12 LVDSs that each 4 converted to 24bit to 2 DS90CR486 ?
if yes what I am doing with the 4 left LVDS (each DS90CR486 has…
Other Parts Discussed in Thread: DS90CR486 , DS90CR485 Hi,
we bought a DS90CR486 133MHz 48-bit Deseriallizer and make a PCB board to measure it.
We want our deseriallizer works on DC balance mode.
So we design our BAL pin tied to high, CON1 tied…
Hi Vera,
Does the interface have to be LVDS to 24-bit parallel RGB? I don't believe we have any devices like this that can support a 148.5MHz clock. The closest there is is the DS90CR486 but that only supports up to 133MHz.
Regards,
I.K.
Hello, here is the document I referenced. I should have attached it.
7418.Camera_Link.pdf
I am designing a board that will interface with a camera that has full Camera Link capability. I want to bring that data into an FPGA and then transmit the…
Hi Sakai-san,
I still have not received any update. It seems that we cannot just fix the pinout image without updating the entire datasheet to meet current TI standards, so it may take a long time if it's approved. It would be best for the customer…
Other Parts Discussed in Thread: DS90CR485 , DS90CR287 , DS90CR486 Hi
Can use DS90CR485 EVB to connect DS90CR288 to try function?(Due to here have no DS90CR287 EVB)
Best regards,
Bogey