Part Number: DS90LV032A Other Parts Discussed in Thread: DS90LV001 , SN65LVDS32 , SN65LVDS050 , SN65LVDS33 , SN65LVDS349 , DS90LV012A , SN65MLVD048
ATIA/EIA-644-A standard allows multiple receiver operation and I used DS90LV032A and MAX9180 receivers…
Part Number: SN65LVDM051 Other Parts Discussed in Thread: DS90LV012A Hi folks,
I would like to spread SPI interface from one Master card to 4 slave cards using LVDS bus. My problem is that communication is not reliable enough even CLK frequensy is 12MHz…
Other Parts Discussed in Thread: DS90LV012A I am new to LVDS technology so please correct me if I am wrong. I have a board that has LVDS driver with 100ohm resistor termination. I am trying to provide the output differential signal from the driver to…
The LVDS Owners Manual is a good source for information on LVDS components. Some of the information in the manual definately applies to the DS90LV011A and DS90LV012A. It is important to look at the datasheet specifications for these devices, the datasheet…
Hi Satoshi-san,
DS90LV011A (Tx) => SN65LVDS32 (Rx)
These two devices are spec'd for different maximum data rates, so I think you can use this pair for operation as long as you do not exceed 100 Mbps. The DS90LV011A is spec'd for optimal operation…
Part Number: SN65LVDS179 Other Parts Discussed in Thread: SN65LVDS104 , DS90LV001 Currently we are using this chip to synchronize radars together. We are using three of these chips. One is driving itself and two other chips. The differential receive lines…
Part Number: DS90LV027A Hi,
We are facing some Voltage Level issue with LVDS. In our case we have to setup an LVDS communication with an FPGA EVK to our DUT. DUT LVDS line is 2.5V. The FPGA pins which is available in FMC connectors is at 1.2V level…
Hi Jyothi,
The SN65LVDS822 IC requires a 3V power supply. As per the TIA-EIA-644 standards, All LVDS outputs have a ±350mV swing and an offset of around 1.2V, which is supported by this device .
slla038b.pdf
The RGB display is supported, as the…