Part Number: DS90UB913Q-Q1 Hi, Is it possible to use SerDes for sending only parallel GPIO (let say 7 bit data) over coax/STP cable in vehicle? Since I'm not sending video, is it possible to eliminate Hsync/Vsync signals? Or it's mandatory for the protocol…
Part Number: DS90UB913Q-Q1 I have looked at the datesheet support string format 10 or12bit,My data is 8bit, can I use it?
Detailed as follows:
Camera parameters are as follows: Effective pixel: 1280HX720V Image frame rate: 720P@ 30fPS Video format: YUV422…
Part Number: DS90UB913Q-Q1 Other Parts Discussed in Thread: ISO7821LLS Does TI have any SerDes chips which will comply with EN60601 medical standards?
I'd like to know if there are any SerDes chips that are medical grade? or example, is the DS90UB913 medical…
Part Number: DS90UB913Q-Q1 Hello team,
Could you please provide us the clear EVK schematic of DS90UB913/4Q?
The same issue has been already reported in the other thread. The schematic is on SNLU110.
e2e.ti.com/.../255193
Regards,
Itoh
Part Number: DS90UB913Q-Q1 Team,
Actual camera system looks like the following: DS90UB913Q -> DS90UB914Q For system upgrade (CSI-2 on RCV side) is DS90UB913Q -> DS90UB954 possible? or is DS90UB913A -> DS90UB954 a must? Any TI reference design or…
Part Number: DS90UB913Q-Q1 Hello -
The datasheet says that the PDB pin has an internal pulldown, which means if PDB is not driven externally the DS90UB913Q-Q1 will be in shutdown mode. I need to know what the value of that internal pulldown is, because…
Part Number: DS90UB913A-Q1 Other Parts Discussed in Thread: DS90UB913Q-Q1 , DS90UB914Q-Q1 Tool/software: Message:
Hello,
I'm currently working with the DS90UB913 serializer in a project, and I'm experiencing an issue where the PCLK drops down to 50/25…
Part Number: DS90UB913Q-Q1 in our design, DS90UB913Q & 914 are set in passthrough mode, my program set 914's slave1 & alias slave id to camera's ID address. PCLK is 12MHz
1)when debug the program, I found that I2C communication is not…
Part Number: DS90UB913Q-Q1 Hi
I am currently developing a camera application.
Currently using TI SERDES(913/914) and inquire about the interface.
When ESD test of camera product or ECU product, the image is shaken little by little. Please inquire if there…
Part Number: DS90UB913Q-Q1 Dear Team,
what is the max range of FDP Link III and under what circumstances? FDP II should go as far as 100m I believe.
Regards
Andreas