Part Number: DS90UB921-Q1
Hello,
Customer is asking for an alternative to DS90UB921TRHSRQ1 in order to manage the shortage.
Do you have a pin2pin serializer that can be a good fit ? DS90UB925-Q1 ?
Best regards,
Matisse
Part Number: DS90UB921-Q1 Hi team,
My clients use 921-948. There are two questions about the GPIO configuration of transparent transmission:
1、If the 25th and 26th pins of the 921 are configured as GPIOs, can they be transparently transmitted to the GPIOs…
Part Number: DS90UB940-Q1 It did not specifically mention in the data sheet. However, in table 101 it's listed. If it's supported, are there any specific register bit settings?
Part Number: DS90UB921-Q1 Hello,
When the DS90UB921 is in 24-bit mode, can GPO_REG6 and GPO_REG7 be used as digital output pins? These pins are shared with I2C_DA and I2S_WC.
Since I am not using I2S, I am hoping to use these pins as outputs. Thanks…
Part Number: DS90UB921-Q1 Hello,
I would like to know more about AVMUTE than that in the datasheet. Would you please answer the bleow 3 questions?
Q1: When the Des is in AVMUTE, are HS/VS/DE and PCLK outputs availbale at output pins while all R/G/B outputs…
Part Number: DS90UB921-Q1 Hi TI team,
Does DS90UB921-Q1 support HBR audio formats via I2S port?
Thank you in advance for your support.
Regards,
Abderrahman
Part Number: DS90UB921-Q1 Dear TI Team:
I'm trying to use the internal test pattern generator to test the connection between DS90UB921 and DS90UB928(as follow).
The Display only supports 44MHz, 1152x576@60fps.
I try to test pattern from ds90ub921…
Part Number: DS90UB921-Q1 Hi
Data circulation mode is ,SOC(IMX6)-921-940-Display SOC,
Detailed description of the problem:
1. Water ripple evenly covers the whole display area of AVM; We have ruled out the problem of the data sent by the camera;
2.…
Part Number: DS90UB921-Q1 Hi,
I'd like to know all condition for SCL is keeping Low with no ACK for DS90UB921.
I'm seeing this behavior on SCL of DS90UB921.
Please let me know.
Regards,
Kasuya