Part Number: DS90UB927Q-Q1 I am simulating FPD Link III interface between DS90UB927Q-Q1 and connector (without PoC) for Frequency domain analysis. I wanted to verify Return loss(RL) and Insertion Loss(IL) it with standard limits as per DS90UB927Q-Q1.…
Part Number: DS90UB927Q-Q1 My customer has a lay-out review tomorrow and asked below Q:
We have a layout meeting tomorrow, where we would like to define the length of the traces to lambda/4. So the frequency would help.
we have a question regarding…
Part Number: DS90UB927Q-Q1 Hi ,
Could you please let me know if it’s possible to enable BIST mode via the I2C into the SER only? I can activate it on the DES by targeting register address (0x24) through the SER I2C, but once enabled, I loose I2C communication…
Part Number: DS90UB927Q-Q1 Hello!
We want to use the LVDS output of the iMX95 (NXP) to connect it to the DS90UB927 serializer, so that it eventually reaches an LCD.
To do this we follow this flow: "iMX95 -> LVDS interface -> DS90UB927 serializer ->…
Part Number: DS90UB927Q-Q1 Tool/software:
Hi Team,
The system application is shown as the above diagram. when camera receives the strong light to the dark light, the output 928 signal will lost. then the display is not smooth and will lost frame.…
Part Number: DS90UB927Q-Q1 Tool/software: Hello TI Team,
I have an LVDS video signal source and need to implement the following signal chain:
Convert LVDS to FPD-Link III (serialization)
Deserialize FPD-Link III back to parallel RGB output
…
Part Number: DS90UB927Q-Q1 Tool/software: Hi,
Is it allowed to add a low voltage up to 2V on the pin 8 CAPL12 during ICT test in production with 2mA current limit.
What is the max voltage we can add on this pin 8?
Is this pin protected with ESD…
Part Number: DS90UB927Q-Q1 Other Parts Discussed in Thread: DS90UB925Q-Q1 , DS90UB926Q-Q1 , Tool/software: Dear supporter,
we have used DS90UB925Q-q1 and DS90UB926Q-q1 experience.
in new product, we need to support RGB LCD, but CPU only supply with…
Part Number: DS90UB927Q-Q1 Tool/software: Hi expert,
could you help review the 927 input LVDS CLK jitter, do this test result meet our spec requirement.
Part Number: DS90UB927Q-Q1 Other Parts Discussed in Thread: DS90UB928Q-Q1
Tool/software:
Dear TI engineers!
We are experiencing an issue with I2C forwarding between DS90UB927Q-Q1 and DS90UB928Q-Q1.
The issue happens when PCLK is being changed…