Part Number: DS90UB934-Q1EVM Other Parts Discussed in Thread: DS90UB934-Q1 , ALP Dear Sir,
I have been testing DS90UB934-Q1 EVM + DS90UB933(our board) for using TI LaunchPAD.
But I have a question for setting partner information.
when It connected USB…
Part Number: TIDA-01004 Other Parts Discussed in Thread: DS90UB933-Q1 , DS90UB934-Q1EVM Hi team,
My customer is studying DS90UB933-Q1 now. but no any experience before.
So any easy way can get an image from the sensor?
Can the images captured by the serializer…
Part Number: DS90UB934-Q1EVM Other Parts Discussed in Thread: ALP I have the DS90UB934EVM. The DS90UB933 produced a development board. We are testing with DS90UB934 and DS90UB933. It comes out with the picture attached to the partner Imformation. DS90UB933…
Hello Nandini,
It seems you are using External Oscillator Mode. If a 36MHz oscillator is used as the reference clock for the 933 device, it will output half that frequency on the CLKOUT pin which can be used as a reference clock for the imager.
I do not…
Part Number: DS90UB933-Q1EVM Other Parts Discussed in Thread: ALP Hi Team
My cusromer want to set-up connecting ub954EVM and ub933.
specific problem is: when they read reg 0x5b of 954, b0 (933 ID) can be seen so 954 recognize 933.
However, they can't read…
Part Number: DS90UB933-Q1EVM Other Parts Discussed in Thread: ALP Hi team,
my customer want to connect UB954 with UB933 on both our EVM, using ALP, they cannot see DS90UB933 device profile, even though followed User's guide instruction. would you please…
Part Number: DS90UB933-Q1EVM Other Parts Discussed in Thread: DS90UB913A-CXEVM , Hi Team,
My customer wants to configure 933 to 934. However, how do they design PoC because PoC filter is different from 913A.
On DS90UB913A-CXEVM, Filter L is 4.7uH + 100uH…
Part Number: DS90UB933-Q1EVM Hi team,
My customer want to clarify if AC coupled capacitor shall be rated 50V. Customer want to use smaller size capacitor which has 16V, not 50V rating?
Is it possible? Regards, NY
Part Number: DS90UB934-Q1 Other Parts Discussed in Thread: DS90UB933-Q1EVM Hi team,
Here's an issue from the customer may need your help:
Connection method (using coax cable): Image sensor--DS90UB933--DS90UB934. And the 933 PCLK is from the image…