Hi FuGuojia,
guojia fu said: Yes,I'm sure the 941 is getting programmed with setting values, I changed Ub941Ub925Config buff with my value.
Ok, understood
guojia fu said: In addition, where is the device tree of DSI? Does it need to be modified…
Part Number: DS90UB941AS-Q1 Tool/software: Hi team,
During vehicle testing, I'm experiencing a DS90UB941AS-Q1 FPD3_LINK_RDY=0 error. I'm wondering: 1. What's the specific detection mechanism for this? 2. Under what circumstances would this register…
Hi Ragav ,
Thank you for your patience in answering questions. We are waiting for some feedback from customers.
The customer is currently confirming and will reply to you shortly.
Ragav Subramanian said: Can you confirm if the fault occurs with…
Part Number: DS90UB941AS-Q1 Dears:
customer has below quesiton need BU help check:
1. In DE (Data Enable) Mode, do the Ser (941) and Des (948) detect HSync/VSync polarity? Does the polarity configuration affect the SerDes link?
2. Under the default…
Part Number: DS90UB941AS-Q1 We have an application where we want to go from MIPI-DSI to FPD-Link <> COAX <> FPD-Link to MIPI-DSI.
The idea is that the SOC outputs native MIPI-DSI and the remote display is dumb, no processor on the display, just FPD…
Part Number: DS90UB941AS-Q1 Other Parts Discussed in Thread: DS90UB984-Q1 Tool/software: Hi,
we are using DS90UB941AS-Q1 in dual output mode for vehicle display interface using power over coaxial (PoC) concept using TE 4P MATE-AX connector.
We would…
Part Number: DS90UB941AS-Q1 Tool/software: When DS90UB941AS-Q1 is connected to two remote deserializers in splitter or independent mode which have the same physical I2C address, how can they be accessed independently via I2C?
question 1:
I refer…
Part Number: DS90UB941AS-Q1 Tool/software: Hi Team,
My customer is looking for any kind of layout recommendation app note or checklist for FPD-Link? They are using the DS90UB941AS-Q1, DS90UB947, and DS90UB948. Anything you can provide would be very…
Hi,
Josh Baik said: Have you checked if it is enabled PATGEN with internal timing and an external clock from 941AS?
I don't think the register configuration is a priority at this point. Before further investigation about the hardware issue, please…