Part Number: DS90UB947-Q1
Tool/software:
Hello, We are planning to use the DS90UB947-Q1 serializer, which supports dual-channel LVDS with 8 lanes (inverting and true LVDS inputs). The SoC we are planning to use, however, provides a single-channel LVDS…
Part Number: DS90UB947-Q1 Tool/software: Hi team,
customer use DS90UB947-Q1 in an IVI project and find that there is screen flickering when working high temperature environment 600h. And customer conduct ABA test, the problem follow DS90UB947-Q1. For now…
Part Number: DS90UB947-Q1 Tool/software: Hi team,
I would like to double check whether DS90UB947-Q1 can support thermal shock test (-40C to 85C) ?
customer conduct the thermal shock test (-40C to 85C) per car end customer requirement, and find there are…
Part Number: DS90UB947-Q1 Tool/software: Hi team,
I can find power up sequence in datasheet, but can't fine power down sequence.
Is there any requirement for power down sequence?
Regards,
Youhei MIYAOKA
Part Number: DS90UB947-Q1 Tool/software: Hi team,
My customer do not use GPIO pins, but it seems to be Input by default. If they do not set the registers as it is, should the GPIO pins set to H or L? Also, when fixing to L, is it OK to connect directly…
Part Number: DS90UB947-Q1 Tool/software: Hello,
Can DS90UB947 support 2348 x 1080 -13,2'' display for automotive multimedia application? If not please give me compatible part for this application.
Part Number: DS90UB947-Q1 Tool/software: Hi,
Currently I am trying to find a solution to convert eDP (2560x1440@60Hz) to MIPI CSI-2 signal, is there any solution to do this?
I noticed that in previous threads, someone said that we could use UB947->UB940…
Part Number: DS90UB947-Q1 Tool/software: Hi team,
I want to check register setting for SCL High/Low Time. Could you check below procedure is correct or not.
They want to set I2C frequency 400kHz. In this case, cycle time is 2.5us and CLK high time is…
Part Number: DS90UB947-Q1 Other Parts Discussed in Thread: PCA9539 Tool/software: Have DS90UB947-Q1 placed on one I2C bus with several devices. It's able to find all I2C devices (e.g. PCA9539) except DS90UB947.
I2C baud rate is 200K. Does anyone have…