Part Number: DS90UB948-Q1 Other Parts Discussed in Thread: DS90UB947-Q1
Hello, I am having a project about ds90ub947q1 and ds90ub948q1. I am reading ds90ub948-q1.pdf and ds90ub948-q1.pdf and I am having questions about 2 pins LOCK and PASS on ds90ub948q1…
Part Number: DS90UB947-Q1 Hi E2E,
When we design products, we need to match Deserializer IC such as DS90UB948.
We want to know how to recognize when a serdes error triggers an interrupt.
We see the combination function of INTB and INTB_IN, but we are…
Part Number: DS90UB947-Q1 Hello,
I am using the EVM DS90UB947 encoder board as a pattern generator, and it is working well with the '946 and '948 decoder boards.
I will be creating a new Printed Circuit Board as part pf a text fixture, board space…
Part Number: DS90UB947-Q1 Hi team,
The customer currently uses the dual PORT inputs of 947. LVDS shares a set of clock inputs. I understand that D0- and D0+ must be of equal length. On the same port, for example: Within what error do the trace lengths of…
Part Number: DS90UB947-Q1 Hi,
Please also help with the following questions. Thank you. How to set up the LVDS part?(As shown in the attachment). What parameters need to be modified in the I2C register part?
LVDS.rar
Jon,
I am not sure what you are trying to show here. Can you please respond to my previous inquiry?
Casey McCrea said: Can you please share a picture of the total setup as well as pictures of the top side markings of the 947 and 948?
Best Regards,
Cas…
Part Number: DS90UB947-Q1 Other Parts Discussed in Thread: DLPC230-Q1 Hi,
I have two openLDI questions want to confirm:
1. I tjit listed in DS90UB947-Q1 datasheet (figure1) is the "input data position" defined in dlpc230-Q1 datasheet (figure2), right? as…
Part Number: DS90UB947-Q1 hi Team,
SAIC EP39 project DMH model use 947+948, now receive SAIC back-end information, the vehicle during the customer use of the vertical line of projection screen problem;
Details are as follows: (1) The occurrence of malfunction…
Part Number: DS90UB947-Q1 Hi team,
For UB948 AC-coupling cap selection, how to understand below screenshot? Is it a typo, both items are for RIN[1:0]+?
For UB947, what should we do for Dout1- and Dout1+ if we only use 1 link FPD-LINK output and work…
Part Number: DS90UB947-Q1 Hi,
My IVI project design with ser 947 and des 940, 947and 940 only use SPI to communicate, no image need to transmit and no image input to 947. I use 947's internal clock for pclk,make 940 lock to 947.940 use for instrument…